MIPI camera driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI camera driver

Jump to solution
4,109 Views
JohnnyK
Contributor I

Hi

I am going to implement a interface to a AR0234CS camera on a iMX1176DV using MIPI interface.

I have made software fore many years, but this is my first time on a iMX platform.

The project I have to implement the interface into, has some MIPI definitions, but no MIPI libraries or interfaces.

Are there any examples or project start code generator to make the interface?

Thank you for your help.

Br Johnny

0 Kudos
Reply
1 Solution
4,093 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.

You can use the SDK examples as reference: https://mcuxpresso.nxp.com/en/welcome 
This application note also can be helpful, it has a chapter that explains the usage of MIPI-CSI example: https://www.nxp.com/docs/en/application-note/AN13573.pdf

If you have more questions do not hesitate to ask me.
Best regards,
Omar

View solution in original post

0 Kudos
Reply
3 Replies
4,089 Views
JohnnyK
Contributor I

Thank you Omar, I will look into that.

Have a great day

Br Johnny

0 Kudos
Reply
4,094 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.

You can use the SDK examples as reference: https://mcuxpresso.nxp.com/en/welcome 
This application note also can be helpful, it has a chapter that explains the usage of MIPI-CSI example: https://www.nxp.com/docs/en/application-note/AN13573.pdf

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 Kudos
Reply
3,774 Views
JohnnyK
Contributor I
Hi Omar
Would you have any example code for connecting an CSI parallel camera to the iMX1176DV?
I tried to toggle the VID_MUX_CTRL to make it take data from parallel input instead of CSI2, but that is not enough.
Hope to get a link to a good example.
Br Johnny
0 Kudos
Reply