MIPI camera driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MIPI camera driver

跳至解决方案
3,837 次查看
JohnnyK
Contributor I

Hi

I am going to implement a interface to a AR0234CS camera on a iMX1176DV using MIPI interface.

I have made software fore many years, but this is my first time on a iMX platform.

The project I have to implement the interface into, has some MIPI definitions, but no MIPI libraries or interfaces.

Are there any examples or project start code generator to make the interface?

Thank you for your help.

Br Johnny

0 项奖励
回复
1 解答
3,821 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.

You can use the SDK examples as reference: https://mcuxpresso.nxp.com/en/welcome 
This application note also can be helpful, it has a chapter that explains the usage of MIPI-CSI example: https://www.nxp.com/docs/en/application-note/AN13573.pdf

If you have more questions do not hesitate to ask me.
Best regards,
Omar

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,817 次查看
JohnnyK
Contributor I

Thank you Omar, I will look into that.

Have a great day

Br Johnny

0 项奖励
回复
3,822 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.

You can use the SDK examples as reference: https://mcuxpresso.nxp.com/en/welcome 
This application note also can be helpful, it has a chapter that explains the usage of MIPI-CSI example: https://www.nxp.com/docs/en/application-note/AN13573.pdf

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 项奖励
回复
3,502 次查看
JohnnyK
Contributor I
Hi Omar
Would you have any example code for connecting an CSI parallel camera to the iMX1176DV?
I tried to toggle the VID_MUX_CTRL to make it take data from parallel input instead of CSI2, but that is not enough.
Hope to get a link to a good example.
Br Johnny
0 项奖励
回复