Hi
I am going to implement a interface to a AR0234CS camera on a iMX1176DV using MIPI interface.
I have made software fore many years, but this is my first time on a iMX platform.
The project I have to implement the interface into, has some MIPI definitions, but no MIPI libraries or interfaces.
Are there any examples or project start code generator to make the interface?
Thank you for your help.
Br Johnny
已解决! 转到解答。
Hello
Hope you are well.
You can use the SDK examples as reference: https://mcuxpresso.nxp.com/en/welcome
This application note also can be helpful, it has a chapter that explains the usage of MIPI-CSI example: https://www.nxp.com/docs/en/application-note/AN13573.pdf
If you have more questions do not hesitate to ask me.
Best regards,
Omar
Hello
Hope you are well.
You can use the SDK examples as reference: https://mcuxpresso.nxp.com/en/welcome
This application note also can be helpful, it has a chapter that explains the usage of MIPI-CSI example: https://www.nxp.com/docs/en/application-note/AN13573.pdf
If you have more questions do not hesitate to ask me.
Best regards,
Omar