remapping ecrypted OTFAD data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

remapping ecrypted OTFAD data

ソリューションへジャンプ
2,075件の閲覧回数
mihaisavu
Contributor I

for IMXRT1170, is it possible to load the same encrypted data in two locations and use remapping, together OTFAD to read one or the other image? Will OTFAD use the remapped address as counter, instead of physical address? 

I want to use external tool to encrypt the data and load the same image in either location. If is possible, please let me know what settings are necessary. 

0 件の賞賛
返信
1 解決策
2,002件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @mihaisavu ,

 

for IMXRT1170, it is possible to load the same encrypted data in two locations and use remapping, and together OTFAD to read either of them depending on remapping is enabled or not, but OTFAD doesn't care about the remapping addresses, it is just used to decrypts any reads from FlexSPI and returns them on the AHB bus.

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,003件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @mihaisavu ,

 

for IMXRT1170, it is possible to load the same encrypted data in two locations and use remapping, and together OTFAD to read either of them depending on remapping is enabled or not, but OTFAD doesn't care about the remapping addresses, it is just used to decrypts any reads from FlexSPI and returns them on the AHB bus.

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
1,966件の閲覧回数
mihaisavu
Contributor I
Hi Kan,
Thanks for your reply. I was hoping there is a way to let OTAFAD know about remapping but it seems there isn't
Regards,
Mihai
0 件の賞賛
返信