remapping ecrypted OTFAD data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

remapping ecrypted OTFAD data

Jump to solution
2,057 Views
mihaisavu
Contributor I

for IMXRT1170, is it possible to load the same encrypted data in two locations and use remapping, together OTFAD to read one or the other image? Will OTFAD use the remapped address as counter, instead of physical address? 

I want to use external tool to encrypt the data and load the same image in either location. If is possible, please let me know what settings are necessary. 

0 Kudos
Reply
1 Solution
1,984 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @mihaisavu ,

 

for IMXRT1170, it is possible to load the same encrypted data in two locations and use remapping, and together OTFAD to read either of them depending on remapping is enabled or not, but OTFAD doesn't care about the remapping addresses, it is just used to decrypts any reads from FlexSPI and returns them on the AHB bus.

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,985 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @mihaisavu ,

 

for IMXRT1170, it is possible to load the same encrypted data in two locations and use remapping, and together OTFAD to read either of them depending on remapping is enabled or not, but OTFAD doesn't care about the remapping addresses, it is just used to decrypts any reads from FlexSPI and returns them on the AHB bus.

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,948 Views
mihaisavu
Contributor I
Hi Kan,
Thanks for your reply. I was hoping there is a way to let OTAFAD know about remapping but it seems there isn't
Regards,
Mihai
0 Kudos
Reply