mimxrt1176avm8a boot mode not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mimxrt1176avm8a boot mode not working

1,293 次查看
irfandelalovic
Contributor I

We are using mimxrt1176avm8a and 128Mb NOR flash connected via flexspi for booting. Program flashed successfully, but code is not executing. Flexspi lines are working during flashing, but clock signal not seen at the start of execution. But the code is working fine using internal RAM. Checked the boot mode pins and it is set to 10 during execution. What may the possible reasons?

 

0 项奖励
回复
3 回复数

1,278 次查看
jay_heng
NXP Employee
NXP Employee

What's the Flexspi pins you used to connect with Flash? what is your Flash device part?

For pin connection, you can refer to FlexSPI NOR连接方式大全(RT1160/1170)

And also you use default \SDK_2.12.1_MIMXRT1170-EVK\boards\evkmimxrt1170\xip\evkmimxrt1170_flexspi_nor_config.c in your project, right?

0 项奖励
回复

1,271 次查看
irfandelalovic
Contributor I
Thank you for the reply,
yes i use it default "\SDK_2.12.1_MIMXRT1170-EVK\boards\evkmimxrt1170\xip\evkmimxrt1170_flexspi_nor_config.c"

 

0 项奖励
回复

1,260 次查看
jay_heng
NXP Employee
NXP Employee

What's the Flexspi pins you used to connect with Flash? what is your Flash device part number?

0 项奖励
回复