mimxrt1176avm8a boot mode not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mimxrt1176avm8a boot mode not working

1,307件の閲覧回数
irfandelalovic
Contributor I

We are using mimxrt1176avm8a and 128Mb NOR flash connected via flexspi for booting. Program flashed successfully, but code is not executing. Flexspi lines are working during flashing, but clock signal not seen at the start of execution. But the code is working fine using internal RAM. Checked the boot mode pins and it is set to 10 during execution. What may the possible reasons?

 

0 件の賞賛
返信
3 返答(返信)

1,292件の閲覧回数
jay_heng
NXP Employee
NXP Employee

What's the Flexspi pins you used to connect with Flash? what is your Flash device part?

For pin connection, you can refer to FlexSPI NOR连接方式大全(RT1160/1170)

And also you use default \SDK_2.12.1_MIMXRT1170-EVK\boards\evkmimxrt1170\xip\evkmimxrt1170_flexspi_nor_config.c in your project, right?

0 件の賞賛
返信

1,285件の閲覧回数
irfandelalovic
Contributor I
Thank you for the reply,
yes i use it default "\SDK_2.12.1_MIMXRT1170-EVK\boards\evkmimxrt1170\xip\evkmimxrt1170_flexspi_nor_config.c"

 

0 件の賞賛
返信

1,274件の閲覧回数
jay_heng
NXP Employee
NXP Employee

What's the Flexspi pins you used to connect with Flash? what is your Flash device part number?

0 件の賞賛
返信