lpspi_interrupt_b2b_master example code concerns

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpspi_interrupt_b2b_master example code concerns

ソリューションへジャンプ
2,622件の閲覧回数
patrick_yang
Contributor I

Hello,

The lpspi_interrupt_b2b_master.c example code confused me about the transfer data frame size and transfer fifo size.

In LPSPI_MasterInit(), the TCR is configured to be the default data frame size, which is 8.  Did not find other statements to change the data frame size to word or 32 bits.  Also

g_masterFifoSize = LPSPI_GetRxFifoSize(EXAMPLE_LPSPI_MASTER_BASEADDR);

where g_masterFifoSize is 16, which shall be 16 * 4 = 64 bytes per the NXP explanation: 

https://community.nxp.com/t5/i-MX-RT/iMX-RT1064-LPSPI-Maximum-FIFO-Size/m-p/915843

 

Below are the confusion statements in the code:

/* Fill up the TX data in FIFO. */
while ((LPSPI_GetTxFifoCount(EXAMPLE_LPSPI_MASTER_BASEADDR) < g_masterFifoSize) &&
(masterTxCount - masterRxCount < g_masterFifoSize))
{
/*Write the word to TX register*/
LPSPI_WriteData(EXAMPLE_LPSPI_MASTER_BASEADDR, masterTxData[masterTxCount]);
++masterTxCount;

if (masterTxCount == TRANSFER_SIZE)
{
break;
}
}

Per the commend, the LPSPI_WriteData() write a word instead of a byte each time.  Per the statements ++masterTxCount; and if (masterTxCount == TRANSFER_SIZE), the LPSPI_WriteData() seems write a byte each time.

 

If LPSPI_WriteData() writes a byte each time and the FIFO buffer size is 64 bytes or 16 words, why using (masterTxCount - masterRxCount < g_masterFifoSize)?  Should it be (masterTxCount - masterRxCount < g_masterFifoSize * 4)?

 

Thank you in advance for any responses.

 

Patrick

0 件の賞賛
返信
1 解決策
2,611件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Firstly, the FIFO depth is 16, and it can store up to 64 bytes, secondly, both 8-bit and 16-bit writes of transmitting data will zero-extend the data written and push the data into the transmit FIFO which is as same as write 32 bit to TDR register.
Hope this is clear.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,612件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Firstly, the FIFO depth is 16, and it can store up to 64 bytes, secondly, both 8-bit and 16-bit writes of transmitting data will zero-extend the data written and push the data into the transmit FIFO which is as same as write 32 bit to TDR register.
Hope this is clear.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,603件の閲覧回数
patrick_yang
Contributor I

Hi, jeremyzhou,

 

Thank you very much for the prompt clarification!

 

Patrick

0 件の賞賛
返信