imx-rt boot pin configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx-rt boot pin configuration

ソリューションへジャンプ
3,613件の閲覧回数
martinribelotta
Contributor I

Hello. I'm starting a development of imx-rt1021 board using as reference the MIMXRT1020HDUG (Hardware Development Guide), the reference manual (IMXRT1020RM)

In IMXRT1020RM, page 292, section 8.4.2 the table 8-4 specifies this pin bootstrap configuration:

pastedImage_1.png

But, in the datasheet (IMXRT1020CEC), page 72, section 5.1, the table 66 is:

pastedImage_2.png

This is consistent with page 8 of hardware reference manual (MIMXRT1020HDUG), Figure 2:

pastedImage_3.png

And the MIMXRT1020-EVK implementation (Sheet 14)

In concret. The BOOT[1:0] is from GPIO_EMC[17:16] or GPIO_AD_B0_[04:03]?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,367件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Martin,

The internal revision concluded that Table 8-4 of the Reference Manual is a mistake. Thanks a lot for your feedback reporting this issue.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,368件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Martin,

The internal revision concluded that Table 8-4 of the Reference Manual is a mistake. Thanks a lot for your feedback reporting this issue.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,367件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Martin,

According with the table of i.MX RT1020 Reference Manual section 4.1.1 “Muxing Options”, the boot select pins are also mapped to GPIO_EMC pins, so it seems to be a typo on Table 8-4.

I have reported this issue, thanks a lot for your feedback. I will post an additional reply when confirming the correct information.


Hope this will be useful for you.
Best regards!
/Carlos

0 件の賞賛
返信