USB recognition error on uClinux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB recognition error on uClinux

2,444 Views
minkyu_shon
Contributor I

Hi.

i.MXRT 1060-EVK based board is under review.

 With the following : 

USB_waveform.png

There are cases when USB is recognized and not. There is a difference in the D+ waveform,

but I want to know the reason for the other part....

The circuit is as follows.

USB_Circuit.png

I'd like you to tell me if there is a problem...

Thanks.....

Labels (1)
0 Kudos
Reply
3 Replies

2,302 Views
minkyu_shon
Contributor I

Hi. Victor....

A Linux (uClinux) Board Support Package is running fine.

booting_picture.png

If you look at the log above, boot is working fine.

Regards,
Shon.

0 Kudos
Reply

2,302 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hi Shon, 

Unfortunately, this board support package is from a third-party provider. I recommend contacting their support line, as they will be able to provide correct information.

If you would like to try our examples please download the SDK. There are several USB examples that can get you started. 
Best Regards, 
Victor 
0 Kudos
Reply

2,302 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hi SON MINKYU, 

The circuit looks fine. Are you running a Linux (uClinux) Board Support package on your board? 

Regards, 

Victor 

0 Kudos
Reply