Secure Boot testing without efusing the signature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Secure Boot testing without efusing the signature

Jump to solution
1,544 Views
Nagaveni
Contributor II

We are using IMX RT 1172
We are using example project for Secure boot
My intention is as below
1. Create hello-world app
2. Secure it with signature
3. test it on board

My problem is due to board limited quantizes, I cannot efuse the signature on the board
Can I use open configuration to test the secure boot functionality with signature verification

0 Kudos
Reply
1 Solution
1,521 Views
jeremyzhou
NXP Employee
NXP Employee

Hi @Nagaveni ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Can I use open configuration to test the secure boot functionality with signature verification
-- No, I'm afraid not, in my opinion, I'd like to suggest not enabling the HAB boot in the design phase.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,522 Views
jeremyzhou
NXP Employee
NXP Employee

Hi @Nagaveni ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Can I use open configuration to test the secure boot functionality with signature verification
-- No, I'm afraid not, in my opinion, I'd like to suggest not enabling the HAB boot in the design phase.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply