Possible error in DCD.c file for RT117x ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Possible error in DCD.c file for RT117x ?

1,667 次查看
carstengroen
Senior Contributor II

In my quest for bringing my own (RT1171) boards up using only 16 bit SDRAM, I'm modifying the DCD.c file (SDK 2.9.2). During this session, I stumbled upon 2 things I don't understand in the DCD settings

  1. GPIO_EMC_B2_17 is used for the signal SEMC_DM3. But there is no PAD control command for this pin (the list stops at GPIO_EMC_B2_16). Is this not missing ?
  2. GPIO_SD_B2_02, GPIO_SD_B2_03,GPIO_SD_B2_04 and GPIO_SD_B2_05 have their PAD control set. However, there is no MUX commands for the pins (the pins controls FlexSPI_B_D1, FlexSPI_B_D0, FlexSPI_B_Clk and FlexSPI_A_DQS, and I don't these are needed ?

I'm not sure if these 2 things are an error or me not being able to figure out why they handled that way.

 

 

 

/*
 * Copyright 2020-2021 NXP
 * All rights reserved.
 *
 * SPDX-License-Identifier: BSD-3-Clause
 */

/***********************************************************************************************************************
 * This file was generated by the MCUXpresso Config Tools. Any manual edits made to this file
 * will be overwritten if the respective MCUXpresso Config Tools is used to update this file.
 **********************************************************************************************************************/

#include "dcd.h"

/* Component ID definition, used by tools. */
#ifndef FSL_COMPONENT_ID
#define FSL_COMPONENT_ID "platform.drivers.xip_board"
#endif

#if defined(XIP_BOOT_HEADER_ENABLE) && (XIP_BOOT_HEADER_ENABLE == 1)
#if defined(XIP_BOOT_HEADER_DCD_ENABLE) && (XIP_BOOT_HEADER_DCD_ENABLE == 1)
#if defined(__CC_ARM) || defined(__ARMCC_VERSION) || defined(__GNUC__)
__attribute__((section(".boot_hdr.dcd_data"), used))
#elif defined(__ICCARM__)
#pragma location = ".boot_hdr.dcd_data"
#endif

/* TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************
!!GlobalInfo
product: DCDx V2.0
processor: MIMXRT1176xxxxx
package_id: MIMXRT1176DVMAA
mcu_data: ksdk2_0
processor_version: 0.0.0
output_format: c_array
 * BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS **********/
/* COMMENTS BELOW ARE USED AS SETTINGS FOR DCD DATA */
const uint8_t dcd_data[] = {
	/* HEADER */
	/* Tag */
	0xD2,
	/* Image Length */
	0x05, 0x08,
	/* Version */
	0x41,

	/* COMMANDS */

	/* group: 'Imported Commands' */
	/* #1.1-139, command header bytes for merged 'Write - value' command */
	0xCC, 0x04, 0x5C, 0x04,
	/* #1.1, command: write_value, address: CCM_CLOCK_ROOT4_CONTROL, value: 0x703, size: 4 */
	0x40, 0xCC, 0x02, 0x00, 0x00, 0x00, 0x07, 0x03,
	/* #1.2, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_00, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x10, 0x00, 0x00, 0x00, 0x00,
	/* #1.3, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_01, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x14, 0x00, 0x00, 0x00, 0x00,
	/* #1.4, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_02, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x18, 0x00, 0x00, 0x00, 0x00,
	/* #1.5, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_03, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x1C, 0x00, 0x00, 0x00, 0x00,
	/* #1.6, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_04, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x20, 0x00, 0x00, 0x00, 0x00,
	/* #1.7, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_05, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x24, 0x00, 0x00, 0x00, 0x00,
	/* #1.8, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_06, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x28, 0x00, 0x00, 0x00, 0x00,
	/* #1.9, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_07, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x2C, 0x00, 0x00, 0x00, 0x00,
	/* #1.10, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_08, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x30, 0x00, 0x00, 0x00, 0x00,
	/* #1.11, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_09, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x34, 0x00, 0x00, 0x00, 0x00,
	/* #1.12, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_10, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x38, 0x00, 0x00, 0x00, 0x00,
	/* #1.13, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_11, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x3C, 0x00, 0x00, 0x00, 0x00,
	/* #1.14, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_12, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x40, 0x00, 0x00, 0x00, 0x00,
	/* #1.15, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_13, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x44, 0x00, 0x00, 0x00, 0x00,
	/* #1.16, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_14, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x48, 0x00, 0x00, 0x00, 0x00,
	/* #1.17, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_15, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x4C, 0x00, 0x00, 0x00, 0x00,
	/* #1.18, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_16, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x50, 0x00, 0x00, 0x00, 0x00,
	/* #1.19, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_17, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x54, 0x00, 0x00, 0x00, 0x00,
	/* #1.20, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_18, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x58, 0x00, 0x00, 0x00, 0x00,
	/* #1.21, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_19, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x5C, 0x00, 0x00, 0x00, 0x00,
	/* #1.22, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_20, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x60, 0x00, 0x00, 0x00, 0x00,
	/* #1.23, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_21, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x64, 0x00, 0x00, 0x00, 0x00,
	/* #1.24, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_22, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x68, 0x00, 0x00, 0x00, 0x00,
	/* #1.25, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_23, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x6C, 0x00, 0x00, 0x00, 0x00,
	/* #1.26, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_24, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x70, 0x00, 0x00, 0x00, 0x00,
	/* #1.27, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_25, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x74, 0x00, 0x00, 0x00, 0x00,
	/* #1.28, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_26, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x78, 0x00, 0x00, 0x00, 0x00,
	/* #1.29, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_27, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x7C, 0x00, 0x00, 0x00, 0x00,
	/* #1.30, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_28, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x80, 0x00, 0x00, 0x00, 0x00,
	/* #1.31, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_29, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x84, 0x00, 0x00, 0x00, 0x00,
	/* #1.32, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_30, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x88, 0x00, 0x00, 0x00, 0x00,
	/* #1.33, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_31, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x8C, 0x00, 0x00, 0x00, 0x00,
	/* #1.34, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_32, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x90, 0x00, 0x00, 0x00, 0x00,
	/* #1.35, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_33, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x94, 0x00, 0x00, 0x00, 0x00,
	/* #1.36, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_34, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x98, 0x00, 0x00, 0x00, 0x00,
	/* #1.37, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_35, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0x9C, 0x00, 0x00, 0x00, 0x00,
	/* #1.38, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_36, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xA0, 0x00, 0x00, 0x00, 0x00,
	/* #1.39, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_37, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xA4, 0x00, 0x00, 0x00, 0x00,
	/* #1.40, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_38, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xA8, 0x00, 0x00, 0x00, 0x00,
	/* #1.41, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_39, value: 0x10, size: 4 */
	0x40, 0x0E, 0x80, 0xAC, 0x00, 0x00, 0x00, 0x10,
	/* #1.42, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_40, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xB0, 0x00, 0x00, 0x00, 0x00,
	/* #1.43, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B1_41, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xB4, 0x00, 0x00, 0x00, 0x00,
	/* #1.44, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_00, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xB8, 0x00, 0x00, 0x00, 0x00,
	/* #1.45, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_01, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xBC, 0x00, 0x00, 0x00, 0x00,
	/* #1.46, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_02, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xC0, 0x00, 0x00, 0x00, 0x00,
	/* #1.47, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_03, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xC4, 0x00, 0x00, 0x00, 0x00,
	/* #1.48, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_04, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xC8, 0x00, 0x00, 0x00, 0x00,
	/* #1.49, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_05, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xCC, 0x00, 0x00, 0x00, 0x00,
	/* #1.50, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_06, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xD0, 0x00, 0x00, 0x00, 0x00,
	/* #1.51, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_07, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xD4, 0x00, 0x00, 0x00, 0x00,
	/* #1.52, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_08, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xD8, 0x00, 0x00, 0x00, 0x00,
	/* #1.53, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_09, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xDC, 0x00, 0x00, 0x00, 0x00,
	/* #1.54, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_10, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xE0, 0x00, 0x00, 0x00, 0x00,
	/* #1.55, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_11, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xE4, 0x00, 0x00, 0x00, 0x00,
	/* #1.56, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_12, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xE8, 0x00, 0x00, 0x00, 0x00,
	/* #1.57, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_13, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xEC, 0x00, 0x00, 0x00, 0x00,
	/* #1.58, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_14, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xF0, 0x00, 0x00, 0x00, 0x00,
	/* #1.59, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_15, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xF4, 0x00, 0x00, 0x00, 0x00,
	/* #1.60, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_16, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xF8, 0x00, 0x00, 0x00, 0x00,
	/* #1.61, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_17, value: 0x00, size: 4 */
	0x40, 0x0E, 0x80, 0xFC, 0x00, 0x00, 0x00, 0x00,
	/* #1.62, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_18, value: 0x00, size: 4 */
	0x40, 0x0E, 0x81, 0x00, 0x00, 0x00, 0x00, 0x00,
	/* #1.63, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_19, value: 0x00, size: 4 */
	0x40, 0x0E, 0x81, 0x04, 0x00, 0x00, 0x00, 0x00,
	/* #1.64, command: write_value, address: IOMUXC_SW_MUX_CTL_PAD_GPIO_EMC_B2_20, value: 0x00, size: 4 */
	0x40, 0x0E, 0x81, 0x08, 0x00, 0x00, 0x00, 0x00,
	/* #1.65, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_00, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0x54, 0x00, 0x00, 0x00, 0x08,
	/* #1.66, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_01, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0x58, 0x00, 0x00, 0x00, 0x08,
	/* #1.67, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_02, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0x5C, 0x00, 0x00, 0x00, 0x08,
	/* #1.68, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_03, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0x60, 0x00, 0x00, 0x00, 0x08,
	/* #1.69, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_04, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0x64, 0x00, 0x00, 0x00, 0x08,
	/* #1.70, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_05, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0x68, 0x00, 0x00, 0x00, 0x08,
	/* #1.71, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_06, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0x6C, 0x00, 0x00, 0x00, 0x08,
	/* #1.72, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_07, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0x70, 0x00, 0x00, 0x00, 0x08,
	/* #1.73, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_08, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0x74, 0x00, 0x00, 0x00, 0x08,
	/* #1.74, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_09, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0x78, 0x00, 0x00, 0x00, 0x08,
	/* #1.75, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_10, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0x7C, 0x00, 0x00, 0x00, 0x08,
	/* #1.76, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_11, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0x80, 0x00, 0x00, 0x00, 0x08,
	/* #1.77, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_12, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0x84, 0x00, 0x00, 0x00, 0x08,
	/* #1.78, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_13, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0x88, 0x00, 0x00, 0x00, 0x08,
	/* #1.79, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_14, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0x8C, 0x00, 0x00, 0x00, 0x08,
	/* #1.80, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_15, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0x90, 0x00, 0x00, 0x00, 0x08,
	/* #1.81, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_16, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0x94, 0x00, 0x00, 0x00, 0x08,
	/* #1.82, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_17, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0x98, 0x00, 0x00, 0x00, 0x08,
	/* #1.83, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_18, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0x9C, 0x00, 0x00, 0x00, 0x08,
	/* #1.84, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_19, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xA0, 0x00, 0x00, 0x00, 0x08,
	/* #1.85, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_20, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xA4, 0x00, 0x00, 0x00, 0x08,
	/* #1.86, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_21, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xA8, 0x00, 0x00, 0x00, 0x08,
	/* #1.87, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_22, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xAC, 0x00, 0x00, 0x00, 0x08,
	/* #1.88, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_23, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xB0, 0x00, 0x00, 0x00, 0x08,
	/* #1.89, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_24, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xB4, 0x00, 0x00, 0x00, 0x08,
	/* #1.90, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_25, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xB8, 0x00, 0x00, 0x00, 0x08,
	/* #1.91, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_26, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xBC, 0x00, 0x00, 0x00, 0x08,
	/* #1.92, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_27, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xC0, 0x00, 0x00, 0x00, 0x08,
	/* #1.93, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_28, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xC4, 0x00, 0x00, 0x00, 0x08,
	/* #1.94, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_29, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xC8, 0x00, 0x00, 0x00, 0x08,
	/* #1.95, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_30, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xCC, 0x00, 0x00, 0x00, 0x08,
	/* #1.96, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_31, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xD0, 0x00, 0x00, 0x00, 0x08,
	/* #1.97, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_32, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xD4, 0x00, 0x00, 0x00, 0x08,
	/* #1.98, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_33, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xD8, 0x00, 0x00, 0x00, 0x08,
	/* #1.99, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_34, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xDC, 0x00, 0x00, 0x00, 0x08,
	/* #1.100, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_35, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xE0, 0x00, 0x00, 0x00, 0x08,
	/* #1.101, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_36, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xE4, 0x00, 0x00, 0x00, 0x08,
	/* #1.102, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_37, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xE8, 0x00, 0x00, 0x00, 0x08,
	/* #1.103, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_38, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xEC, 0x00, 0x00, 0x00, 0x08,
	/* #1.104, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_39, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xF0, 0x00, 0x00, 0x00, 0x08,
	/* #1.105, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_40, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xF4, 0x00, 0x00, 0x00, 0x08,
	/* #1.106, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B1_41, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xF8, 0x00, 0x00, 0x00, 0x08,
	/* #1.107, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_00, value: 0x08, size: 4 */
	0x40, 0x0E, 0x82, 0xFC, 0x00, 0x00, 0x00, 0x08,
	/* #1.108, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_01, value: 0x08, size: 4 */
	0x40, 0x0E, 0x83, 0x00, 0x00, 0x00, 0x00, 0x08,
	/* #1.109, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_02, value: 0x08, size: 4 */
	0x40, 0x0E, 0x83, 0x04, 0x00, 0x00, 0x00, 0x08,
	/* #1.110, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_03, value: 0x08, size: 4 */
	0x40, 0x0E, 0x83, 0x08, 0x00, 0x00, 0x00, 0x08,
	/* #1.111, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_04, value: 0x08, size: 4 */
	0x40, 0x0E, 0x83, 0x0C, 0x00, 0x00, 0x00, 0x08,
	/* #1.112, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_05, value: 0x08, size: 4 */
	0x40, 0x0E, 0x83, 0x10, 0x00, 0x00, 0x00, 0x08,
	/* #1.113, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_06, value: 0x08, size: 4 */
	0x40, 0x0E, 0x83, 0x14, 0x00, 0x00, 0x00, 0x08,
	/* #1.114, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_07, value: 0x08, size: 4 */
	0x40, 0x0E, 0x83, 0x18, 0x00, 0x00, 0x00, 0x08,
	/* #1.115, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_08, value: 0x08, size: 4 */
	0x40, 0x0E, 0x83, 0x1C, 0x00, 0x00, 0x00, 0x08,
	/* #1.116, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_09, value: 0x08, size: 4 */
	0x40, 0x0E, 0x83, 0x20, 0x00, 0x00, 0x00, 0x08,
	/* #1.117, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_10, value: 0x08, size: 4 */
	0x40, 0x0E, 0x83, 0x24, 0x00, 0x00, 0x00, 0x08,
	/* #1.118, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_11, value: 0x08, size: 4 */
	0x40, 0x0E, 0x83, 0x28, 0x00, 0x00, 0x00, 0x08,
	/* #1.119, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_12, value: 0x08, size: 4 */
	0x40, 0x0E, 0x83, 0x2C, 0x00, 0x00, 0x00, 0x08,
	/* #1.120, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_13, value: 0x08, size: 4 */
	0x40, 0x0E, 0x83, 0x30, 0x00, 0x00, 0x00, 0x08,
	/* #1.121, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_14, value: 0x08, size: 4 */
	0x40, 0x0E, 0x83, 0x34, 0x00, 0x00, 0x00, 0x08,
	/* #1.122, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_15, value: 0x08, size: 4 */
	0x40, 0x0E, 0x83, 0x38, 0x00, 0x00, 0x00, 0x08,
	/* #1.123, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_16, value: 0x08, size: 4 */
	0x40, 0x0E, 0x83, 0x3C, 0x00, 0x00, 0x00, 0x08,
	/* #1.124, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_SD_B2_02, value: 0x08, size: 4 */
	0x40, 0x0E, 0x84, 0x00, 0x00, 0x00, 0x00, 0x08,
	/* #1.125, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_SD_B2_03, value: 0x08, size: 4 */
	0x40, 0x0E, 0x84, 0x04, 0x00, 0x00, 0x00, 0x08,
	/* #1.126, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_SD_B2_04, value: 0x08, size: 4 */
	0x40, 0x0E, 0x84, 0x08, 0x00, 0x00, 0x00, 0x08,
	/* #1.127, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_SD_B2_05, value: 0x08, size: 4 */
	0x40, 0x0E, 0x84, 0x0C, 0x00, 0x00, 0x00, 0x08,
	/* #1.128, command: write_value, address: SEMC_MCR, value: 0x10000004, size: 4 */
	0x40, 0x0D, 0x40, 0x00, 0x10, 0x00, 0x00, 0x04,
	/* #1.129, command: write_value, address: SEMC_BMCR0, value: 0x81, size: 4 */
	0x40, 0x0D, 0x40, 0x08, 0x00, 0x00, 0x00, 0x81,
	/* #1.130, command: write_value, address: SEMC_BMCR1, value: 0x81, size: 4 */
	0x40, 0x0D, 0x40, 0x0C, 0x00, 0x00, 0x00, 0x81,
	/* #1.131, command: write_value, address: SEMC_BR0, value: 0x8000001D, size: 4 */
	0x40, 0x0D, 0x40, 0x10, 0x80, 0x00, 0x00, 0x1D,
	/* #1.132, command: write_value, address: SEMC_SDRAMCR0, value: 0xF32, size: 4 */
	0x40, 0x0D, 0x40, 0x40, 0x00, 0x00, 0x0F, 0x32,
	/* #1.133, command: write_value, address: SEMC_SDRAMCR1, value: 0x772A22, size: 4 */
	0x40, 0x0D, 0x40, 0x44, 0x00, 0x77, 0x2A, 0x22,
	/* #1.134, command: write_value, address: SEMC_SDRAMCR2, value: 0x10A0D, size: 4 */
	0x40, 0x0D, 0x40, 0x48, 0x00, 0x01, 0x0A, 0x0D,
	/* #1.135, command: write_value, address: SEMC_SDRAMCR3, value: 0x21210408, size: 4 */
	0x40, 0x0D, 0x40, 0x4C, 0x21, 0x21, 0x04, 0x08,
	/* #1.136, command: write_value, address: SEMC_IPCR0, value: 0x80000000, size: 4 */
	0x40, 0x0D, 0x40, 0x90, 0x80, 0x00, 0x00, 0x00,
	/* #1.137, command: write_value, address: SEMC_IPCR1, value: 0x02, size: 4 */
	0x40, 0x0D, 0x40, 0x94, 0x00, 0x00, 0x00, 0x02,
	/* #1.138, command: write_value, address: SEMC_IPCR2, value: 0x00, size: 4 */
	0x40, 0x0D, 0x40, 0x98, 0x00, 0x00, 0x00, 0x00,
	/* #1.139, command: write_value, address: SEMC_IPCMD, value: 0xA55A000F, size: 4 */
	0x40, 0x0D, 0x40, 0x9C, 0xA5, 0x5A, 0x00, 0x0F,
	/* #2, command: nop */
	0xC0, 0x00, 0x04, 0x00,
	/* #3, command: nop */
	0xC0, 0x00, 0x04, 0x00,
	/* #4, command: nop */
	0xC0, 0x00, 0x04, 0x00,
	/* #5, command: nop */
	0xC0, 0x00, 0x04, 0x00,
	/* #6, command: nop */
	0xC0, 0x00, 0x04, 0x00,
	/* #7.1-2, command header bytes for merged 'Write - value' command */
	0xCC, 0x00, 0x14, 0x04,
	/* #7.1, command: write_value, address: SEMC_INTR, value: 0x03, size: 4 */
	0x40, 0x0D, 0x40, 0x3C, 0x00, 0x00, 0x00, 0x03,
	/* #7.2, command: write_value, address: SEMC_IPCMD, value: 0xA55A000C, size: 4 */
	0x40, 0x0D, 0x40, 0x9C, 0xA5, 0x5A, 0x00, 0x0C,
	/* #8, command: nop */
	0xC0, 0x00, 0x04, 0x00,
	/* #9, command: nop */
	0xC0, 0x00, 0x04, 0x00,
	/* #10, command: nop */
	0xC0, 0x00, 0x04, 0x00,
	/* #11, command: nop */
	0xC0, 0x00, 0x04, 0x00,
	/* #12, command: nop */
	0xC0, 0x00, 0x04, 0x00,
	/* #13.1-2, command header bytes for merged 'Write - value' command */
	0xCC, 0x00, 0x14, 0x04,
	/* #13.1, command: write_value, address: SEMC_INTR, value: 0x03, size: 4 */
	0x40, 0x0D, 0x40, 0x3C, 0x00, 0x00, 0x00, 0x03,
	/* #13.2, command: write_value, address: SEMC_IPCMD, value: 0xA55A000C, size: 4 */
	0x40, 0x0D, 0x40, 0x9C, 0xA5, 0x5A, 0x00, 0x0C,
	/* #14, command: nop */
	0xC0, 0x00, 0x04, 0x00,
	/* #15, command: nop */
	0xC0, 0x00, 0x04, 0x00,
	/* #16, command: nop */
	0xC0, 0x00, 0x04, 0x00,
	/* #17, command: nop */
	0xC0, 0x00, 0x04, 0x00,
	/* #18, command: nop */
	0xC0, 0x00, 0x04, 0x00,
	/* #19.1-3, command header bytes for merged 'Write - value' command */
	0xCC, 0x00, 0x1C, 0x04,
	/* #19.1, command: write_value, address: SEMC_INTR, value: 0x03, size: 4 */
	0x40, 0x0D, 0x40, 0x3C, 0x00, 0x00, 0x00, 0x03,
	/* #19.2, command: write_value, address: SEMC_IPTXDAT, value: 0x33, size: 4 */
	0x40, 0x0D, 0x40, 0xA0, 0x00, 0x00, 0x00, 0x33,
	/* #19.3, command: write_value, address: SEMC_IPCMD, value: 0xA55A000A, size: 4 */
	0x40, 0x0D, 0x40, 0x9C, 0xA5, 0x5A, 0x00, 0x0A,
	/* #20, command: nop */
	0xC0, 0x00, 0x04, 0x00,
	/* #21, command: nop */
	0xC0, 0x00, 0x04, 0x00,
	/* #22, command: nop */
	0xC0, 0x00, 0x04, 0x00,
	/* #23, command: nop */
	0xC0, 0x00, 0x04, 0x00,
	/* #24, command: nop */
	0xC0, 0x00, 0x04, 0x00,
	/* #25.1-2, command header bytes for merged 'Write - value' command */
	0xCC, 0x00, 0x14, 0x04,
	/* #25.1, command: write_value, address: SEMC_INTR, value: 0x03, size: 4 */
	0x40, 0x0D, 0x40, 0x3C, 0x00, 0x00, 0x00, 0x03,
	/* #25.2, command: write_value, address: SEMC_SDRAMCR3, value: 0x21210409, size: 4 */
	0x40, 0x0D, 0x40, 0x4C, 0x21, 0x21, 0x04, 0x09
	};
/* BE CAREFUL MODIFYING THIS SETTINGS - IT IS YAML SETTINGS FOR TOOLS */

#else
const uint8_t dcd_data[] = {0x00};
#endif /* XIP_BOOT_HEADER_DCD_ENABLE */
#endif /* XIP_BOOT_HEADER_ENABLE */

 

 

0 项奖励
回复
3 回复数

1,631 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @carstengroen,

In your first question you mention there isn't a PAD control command for this pin, could you clarify what do you mean about this?

About your second question, the pinmux for the FlexSPI is configured insite the bootROM as it mention in the following flowchart:

Alexis_A_0-1624573502490.png

Best Regards,

Alexis Andalon

 

0 项奖励
回复

1,625 次查看
carstengroen
Senior Contributor II

Hi Alexis,

Regarding item 1:

If you look in the attached DCD code, you will see that there is a bunch of 

IOMUXC_SW_MUX_CTL_PAD_xxxx

statements, these are followed by a bunch of

IOMUXC_SW_PAD_CTL_PAD_xxxx

The first group, the _MUX_ commands, sets the functionality of each of the EMC pins. The second group, the _PAD_ commands, sets the drive level of these EMC pins.

In the first group with the _MUX_ commands, the last pin that is set is pin GPIO_EMC_B2_17, so all the EMC pins have been set correctly (with their MUX)

However, in the second group of commands, with the _PAD_ commands, the last pin that is set is pin GPIO_EMC_B2_16 and pin GPIO_EMC_B2_17 is NOT set in this group of commands. I think this is an error ?

/* #1.123, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_EMC_B2_16, value: 0x08, size: 4 */
	0x40, 0x0E, 0x83, 0x3C, 0x00, 0x00, 0x00, 0x08,

 

Regarding item 2:

I am aware that the pinmux for the FlexSPI is configured inside the bootrom.

But, why are the _PAD_ commands issued in the DCD structure then (there is no corresponding _MUX_ command for these 4 pins in the DCD data, only the _PAD_ commands)?

In the DCD data:

/* #1.124, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_SD_B2_02, value: 0x08, size: 4 */
	0x40, 0x0E, 0x84, 0x00, 0x00, 0x00, 0x00, 0x08,
	/* #1.125, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_SD_B2_03, value: 0x08, size: 4 */
	0x40, 0x0E, 0x84, 0x04, 0x00, 0x00, 0x00, 0x08,
	/* #1.126, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_SD_B2_04, value: 0x08, size: 4 */
	0x40, 0x0E, 0x84, 0x08, 0x00, 0x00, 0x00, 0x08,
	/* #1.127, command: write_value, address: IOMUXC_SW_PAD_CTL_PAD_GPIO_SD_B2_05, value: 0x08, size: 4 */
	0x40, 0x0E, 0x84, 0x0C, 0x00, 0x00, 0x00, 0x08,

 

I hope I explained it better this time

 

 

0 项奖励
回复

1,644 次查看
carstengroen
Senior Contributor II
0 项奖励
回复