I'm using SDK 2.9.2 for RT117x. I have done my own boards with 16 bit SDRAM (single MT48LC16M16 device). CPU is RT1171 at the moment (due to shortage of 1176). Now, in the process of bringing this board up and checking SDRAM in the debugger in Keil, I have stumbled upon an error (I think...)
In the file, evkmimxrt1170_sdram_init.ini the various registers are programmed so the debugger has access to the SDRAM etc. In the function _sdr_init() the IOMUX, PAD control is set
The IOMUX is set correctly for the EMC pins, including EMC_B2_17, EMC_B2_18, EMC_B2_19 and EMC_B2_20. But later in the function where the PAD drive is set, these pins are not set, however EMC_SD_B2_02, EMC_SD_B2_03, EMC_SD_B2_04 and EMC_SD_B2_05 is. I think this is an error (as these signals are used for FlexSPI B and A, and as such has nothing to do with the SDRAM) ?
I have included the (with my comments) the code for the function.
I think the 4 lines for the PAD control should read:
_WDWORD(0x400E8340, 0x00000008); // EMC_B2_17
_WDWORD(0x400E8344, 0x00000008); // EMC_B2_18
_WDWORD(0x400E8348, 0x00000008); // EMC_B2_19
_WDWORD(0x400E834C, 0x00000008); // EMC_B2_20
FUNC void _sdr_Init(void)
{
// Config IOMUX
_WDWORD(0x400E8010, 0x00000000); // EMC_B1_00
_WDWORD(0x400E8014, 0x00000000); // EMC_B1_01
_WDWORD(0x400E8018, 0x00000000); // EMC_B1_02
_WDWORD(0x400E801C, 0x00000000); // EMC_B1_03
_WDWORD(0x400E8020, 0x00000000); // EMC_B1_04
_WDWORD(0x400E8024, 0x00000000); // EMC_B1_05
_WDWORD(0x400E8028, 0x00000000); // EMC_B1_06
_WDWORD(0x400E802C, 0x00000000); // EMC_B1_07
_WDWORD(0x400E8030, 0x00000000); // EMC_B1_08
_WDWORD(0x400E8034, 0x00000000); // EMC_B1_09
_WDWORD(0x400E8038, 0x00000000); // EMC_B1_10
_WDWORD(0x400E803C, 0x00000000); // EMC_B1_11
_WDWORD(0x400E8040, 0x00000000); // EMC_B1_12
_WDWORD(0x400E8044, 0x00000000); // EMC_B1_13
_WDWORD(0x400E8048, 0x00000000); // EMC_B1_14
_WDWORD(0x400E804C, 0x00000000); // EMC_B1_15
_WDWORD(0x400E8050, 0x00000000); // EMC_B1_16
_WDWORD(0x400E8054, 0x00000000); // EMC_B1_17
_WDWORD(0x400E8058, 0x00000000); // EMC_B1_18
_WDWORD(0x400E805C, 0x00000000); // EMC_B1_19
_WDWORD(0x400E8060, 0x00000000); // EMC_B1_20
_WDWORD(0x400E8064, 0x00000000); // EMC_B1_21
_WDWORD(0x400E8068, 0x00000000); // EMC_B1_22
_WDWORD(0x400E806C, 0x00000000); // EMC_B1_23
_WDWORD(0x400E8070, 0x00000000); // EMC_B1_24
_WDWORD(0x400E8074, 0x00000000); // EMC_B1_25
_WDWORD(0x400E8078, 0x00000000); // EMC_B1_26
_WDWORD(0x400E807C, 0x00000000); // EMC_B1_27
_WDWORD(0x400E8080, 0x00000000); // EMC_B1_28
_WDWORD(0x400E8084, 0x00000000); // EMC_B1_29
_WDWORD(0x400E8088, 0x00000000); // EMC_B1_30
_WDWORD(0x400E808C, 0x00000000); // EMC_B1_31
_WDWORD(0x400E8090, 0x00000000); // EMC_B1_32
_WDWORD(0x400E8094, 0x00000000); // EMC_B1_33
_WDWORD(0x400E8098, 0x00000000); // EMC_B1_34
_WDWORD(0x400E809C, 0x00000000); // EMC_B1_35
_WDWORD(0x400E80A0, 0x00000000); // EMC_B1_36
_WDWORD(0x400E80A4, 0x00000000); // EMC_B1_37
_WDWORD(0x400E80A8, 0x00000000); // EMC_B1_38
_WDWORD(0x400E80AC, 0x00000010); // EMC_39, DQS PIN, enable SION
_WDWORD(0x400E80B0, 0x00000000); // EMC_B1_40
_WDWORD(0x400E80B4, 0x00000000); // EMC_B1_41
_WDWORD(0x400E80B8, 0x00000000); // EMC_B2_00
_WDWORD(0x400E80BC, 0x00000000); // EMC_B2_01
_WDWORD(0x400E80C0, 0x00000000); // EMC_B2_02
_WDWORD(0x400E80C4, 0x00000000); // EMC_B2_03
_WDWORD(0x400E80C8, 0x00000000); // EMC_B2_04
_WDWORD(0x400E80CC, 0x00000000); // EMC_B2_05
_WDWORD(0x400E80D0, 0x00000000); // EMC_B2_06
_WDWORD(0x400E80D4, 0x00000000); // EMC_B2_07
_WDWORD(0x400E80D8, 0x00000000); // EMC_B2_08
_WDWORD(0x400E80DC, 0x00000000); // EMC_B2_09
_WDWORD(0x400E80E0, 0x00000000); // EMC_B2_10
_WDWORD(0x400E80E4, 0x00000000); // EMC_B2_11
_WDWORD(0x400E80E8, 0x00000000); // EMC_B2_12
_WDWORD(0x400E80EC, 0x00000000); // EMC_B2_13
_WDWORD(0x400E80F0, 0x00000000); // EMC_B2_14
_WDWORD(0x400E80F4, 0x00000000); // EMC_B2_15
_WDWORD(0x400E80F8, 0x00000000); // EMC_B2_16
_WDWORD(0x400E80FC, 0x00000000); // EMC_B2_17
_WDWORD(0x400E8100, 0x00000000); // EMC_B2_18
_WDWORD(0x400E8104, 0x00000000); // EMC_B2_19
_WDWORD(0x400E8108, 0x00000000); // EMC_B2_20
// PAD ctrl
// PDRV = 1b (normal); PULL = 10b (PD)
_WDWORD(0x400E8254, 0x00000008); // EMC_B1_00
_WDWORD(0x400E8258, 0x00000008); // EMC_B1_01
_WDWORD(0x400E825C, 0x00000008); // EMC_B1_02
_WDWORD(0x400E8260, 0x00000008); // EMC_B1_03
_WDWORD(0x400E8264, 0x00000008); // EMC_B1_04
_WDWORD(0x400E8268, 0x00000008); // EMC_B1_05
_WDWORD(0x400E826C, 0x00000008); // EMC_B1_06
_WDWORD(0x400E8270, 0x00000008); // EMC_B1_07
_WDWORD(0x400E8274, 0x00000008); // EMC_B1_08
_WDWORD(0x400E8278, 0x00000008); // EMC_B1_09
_WDWORD(0x400E827C, 0x00000008); // EMC_B1_10
_WDWORD(0x400E8280, 0x00000008); // EMC_B1_11
_WDWORD(0x400E8284, 0x00000008); // EMC_B1_12
_WDWORD(0x400E8288, 0x00000008); // EMC_B1_13
_WDWORD(0x400E828C, 0x00000008); // EMC_B1_14
_WDWORD(0x400E8290, 0x00000008); // EMC_B1_15
_WDWORD(0x400E8294, 0x00000008); // EMC_B1_16
_WDWORD(0x400E8298, 0x00000008); // EMC_B1_17
_WDWORD(0x400E829C, 0x00000008); // EMC_B1_18
_WDWORD(0x400E82A0, 0x00000008); // EMC_B1_19
_WDWORD(0x400E82A4, 0x00000008); // EMC_B1_20
_WDWORD(0x400E82A8, 0x00000008); // EMC_B1_21
_WDWORD(0x400E82AC, 0x00000008); // EMC_B1_22
_WDWORD(0x400E82B0, 0x00000008); // EMC_B1_23
_WDWORD(0x400E82B4, 0x00000008); // EMC_B1_24
_WDWORD(0x400E82B8, 0x00000008); // EMC_B1_25
_WDWORD(0x400E82BC, 0x00000008); // EMC_B1_26
_WDWORD(0x400E82C0, 0x00000008); // EMC_B1_27
_WDWORD(0x400E82C4, 0x00000008); // EMC_B1_28
_WDWORD(0x400E82C8, 0x00000008); // EMC_B1_29
_WDWORD(0x400E82CC, 0x00000008); // EMC_B1_30
_WDWORD(0x400E82D0, 0x00000008); // EMC_B1_31
_WDWORD(0x400E82D4, 0x00000008); // EMC_B1_32
_WDWORD(0x400E82D8, 0x00000008); // EMC_B1_33
_WDWORD(0x400E82DC, 0x00000008); // EMC_B1_34
_WDWORD(0x400E82E0, 0x00000008); // EMC_B1_35
_WDWORD(0x400E82E4, 0x00000008); // EMC_B1_36
_WDWORD(0x400E82E8, 0x00000008); // EMC_B1_37
_WDWORD(0x400E82EC, 0x00000008); // EMC_B1_38
_WDWORD(0x400E82F0, 0x00000008); // EMC_39, DQS PIN, enable SION
_WDWORD(0x400E82F4, 0x00000008); // EMC_B1_40
_WDWORD(0x400E82F8, 0x00000008); // EMC_B1_41
_WDWORD(0x400E82FC, 0x00000008); // EMC_B2_00
_WDWORD(0x400E8300, 0x00000008); // EMC_B2_01
_WDWORD(0x400E8304, 0x00000008); // EMC_B2_02
_WDWORD(0x400E8308, 0x00000008); // EMC_B2_03
_WDWORD(0x400E830C, 0x00000008); // EMC_B2_04
_WDWORD(0x400E8310, 0x00000008); // EMC_B2_05
_WDWORD(0x400E8314, 0x00000008); // EMC_B2_06
_WDWORD(0x400E8318, 0x00000008); // EMC_B2_07
_WDWORD(0x400E831C, 0x00000008); // EMC_B2_08
_WDWORD(0x400E8320, 0x00000008); // EMC_B2_09
_WDWORD(0x400E8324, 0x00000008); // EMC_B2_10
_WDWORD(0x400E8328, 0x00000008); // EMC_B2_11
_WDWORD(0x400E832C, 0x00000008); // EMC_B2_12
_WDWORD(0x400E8330, 0x00000008); // EMC_B2_13
_WDWORD(0x400E8334, 0x00000008); // EMC_B2_14
_WDWORD(0x400E8338, 0x00000008); // EMC_B2_15
_WDWORD(0x400E833C, 0x00000008); // EMC_B2_16
_WDWORD(0x400E8400, 0x00000008); // EMC_SD_B2_02 <<---- This is an error ? I think these 4 lines should be for EMC_B2_17..EMC_B2_20 instead
_WDWORD(0x400E8404, 0x00000008); // EMC_SD_B2_03
_WDWORD(0x400E8408, 0x00000008); // EMC_SD_B2_04
_WDWORD(0x400E840C, 0x00000008); // EMC_SD_B2_05
// Config SDR Controller Registers/
_WDWORD(0x400d4000,0x10000004); // MCR
_WDWORD(0x400d4008,0x00000081); // BMCR0
_WDWORD(0x400d400C,0x00000081); // BMCR1
//_WDWORD(0x400d4010,0x8000001D); // BR0, 64MB
_WDWORD(0x400d4010,0x8000001B); // BR0, 32MB
//_WDWORD(0x400d4040,0x00000F32); // SDRAMCR0, 32bit
_WDWORD(0x400d4040,0x00000F31); // SDRAMCR0, 16bit
_WDWORD(0x400d4044,0x00772A22); // SDRAMCR1
_WDWORD(0x400d4048,0x00010A0D); // SDRAMCR2
_WDWORD(0x400d404C,0x21210408); // SDRAMCR3
_WDWORD(0x400d4090,0x80000000); // IPCR0
_WDWORD(0x400d4094,0x00000002); // IPCR1
_WDWORD(0x400d4098,0x00000000); // IPCR2
_WDWORD(0x400d409C,0xA55A000F); // IPCMD, SD_CC_IPREA
SDRAM_WaitIpCmdDone();
_WDWORD(0x400d409C,0xA55A000C); // SD_CC_IAF
SDRAM_WaitIpCmdDone();
_WDWORD(0x400d409C,0xA55A000C); // SD_CC_IAF
SDRAM_WaitIpCmdDone();
_WDWORD(0x400d40A0,0x00000033); // IPTXDAT
_WDWORD(0x400d409C,0xA55A000A); // SD_CC_IMS
SDRAM_WaitIpCmdDone();
_WDWORD(0x400d4150,0x00000017); // DCCR
_WDWORD(0x400d404C,0x21210409 ); // enable sdram self refresh again after initialization done.
}