LPSPI Peripheral Chip Select

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPSPI Peripheral Chip Select

ソリューションへジャンプ
3,641件の閲覧回数
Angel487
Contributor I

Hello NXP Community

On my project I need to drive a decoder/demultiplexer with SPI "chip select" pins (Pcs0, Pcs1, Pcs2).

This pins must be all active high (done) and I also need to drive more than one pin high or low.

This last requirement doesn't seem to be provided by the "fsl_lpspi" NXP driver.

I also tried to drive the pins as normal GPIOs, but this results in an out of timing behavior of CS.

Can you please help me?!

Thanks in Advance! 

Angelo

P.S. we are using this logic with de decoder since we have more than 4 chips on the SPI bus (see the attached schematics)

ラベル(1)
0 件の賞賛
返信
1 解決策
3,615件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Angel487 ,

   Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

  I checked the LPSPI IP module, from the register, just can select one PCS pin:

kerryzhou_0-1690782247227.png

TCR register:

kerryzhou_1-1690782256522.png

If you want more than one pin as the SPI_CS function.

Just the LPSPI IP hardware, no register to select it.

So, maybe still need to use the GPIO method.

You mentioned:

I also tried to drive the pins as normal GPIOs, but this results in an out of timing behavior of CS.

What's the detail situation? Which timing behavior is out?

Can you share some wave about it?

If you think the normal GPIO speed is slow, you can use the fast GPIO:

https://www.cnblogs.com/henjay724/p/15518705.html

If just the CS area is not correct, it is related to your GPIO CS code insert area, you need to go to the fsl_lpspi to add it.

 

With it helps you!

Best Regards,

Kerry

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,616件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Angel487 ,

   Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

  I checked the LPSPI IP module, from the register, just can select one PCS pin:

kerryzhou_0-1690782247227.png

TCR register:

kerryzhou_1-1690782256522.png

If you want more than one pin as the SPI_CS function.

Just the LPSPI IP hardware, no register to select it.

So, maybe still need to use the GPIO method.

You mentioned:

I also tried to drive the pins as normal GPIOs, but this results in an out of timing behavior of CS.

What's the detail situation? Which timing behavior is out?

Can you share some wave about it?

If you think the normal GPIO speed is slow, you can use the fast GPIO:

https://www.cnblogs.com/henjay724/p/15518705.html

If just the CS area is not correct, it is related to your GPIO CS code insert area, you need to go to the fsl_lpspi to add it.

 

With it helps you!

Best Regards,

Kerry

 

 

 

0 件の賞賛
返信