Is an external pulldown resistor necessary on the GP input with internal pulldown pin?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is an external pulldown resistor necessary on the GP input with internal pulldown pin?

跳至解决方案
1,033 次查看
Taka05
Contributor I

 

GPIO_B0_04 is a 100kΩ pull-down input pin while MIMXRT1062 reset input POR_B = "L".

Furthermore, even after reset release, the default setting is an input pin with a 100kohm pulldown.

Is an external pulldown resistor(e.g.10kohm) required to use the GPIO_B0_04 as an input pin with pulldown?

Since the internal pulldown is not changed from the RESET state (pulldown 100Kohm), could this internal resistor be effective?

 

标签 (1)
0 项奖励
回复
1 解答
1,018 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Taka05 ,

Please note, the GPIO_B0_04 is the BOOT_CFG[0], so you can refer to the MIMXRT1060-EVK board

kerryzhou_0-1682067574785.pngkerryzhou_1-1682067581471.png

kerryzhou_2-1682067589590.png

 

 

Wish it helps you!

Best Regards,

Kerry

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,019 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Taka05 ,

Please note, the GPIO_B0_04 is the BOOT_CFG[0], so you can refer to the MIMXRT1060-EVK board

kerryzhou_0-1682067574785.pngkerryzhou_1-1682067581471.png

kerryzhou_2-1682067589590.png

 

 

Wish it helps you!

Best Regards,

Kerry

 

0 项奖励
回复