Is an external pulldown resistor necessary on the GP input with internal pulldown pin?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is an external pulldown resistor necessary on the GP input with internal pulldown pin?

Jump to solution
1,042 Views
Taka05
Contributor I

 

GPIO_B0_04 is a 100kΩ pull-down input pin while MIMXRT1062 reset input POR_B = "L".

Furthermore, even after reset release, the default setting is an input pin with a 100kohm pulldown.

Is an external pulldown resistor(e.g.10kohm) required to use the GPIO_B0_04 as an input pin with pulldown?

Since the internal pulldown is not changed from the RESET state (pulldown 100Kohm), could this internal resistor be effective?

 

Labels (1)
0 Kudos
Reply
1 Solution
1,027 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Taka05 ,

Please note, the GPIO_B0_04 is the BOOT_CFG[0], so you can refer to the MIMXRT1060-EVK board

kerryzhou_0-1682067574785.pngkerryzhou_1-1682067581471.png

kerryzhou_2-1682067589590.png

 

 

Wish it helps you!

Best Regards,

Kerry

 

View solution in original post

0 Kudos
Reply
1 Reply
1,028 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Taka05 ,

Please note, the GPIO_B0_04 is the BOOT_CFG[0], so you can refer to the MIMXRT1060-EVK board

kerryzhou_0-1682067574785.pngkerryzhou_1-1682067581471.png

kerryzhou_2-1682067589590.png

 

 

Wish it helps you!

Best Regards,

Kerry

 

0 Kudos
Reply