Hi,
I'm trying to enable instruction trace using i.MXRT1176 trace pins and a J-Trace probe on a MIMXRT1170-EVK board.
I have installed resistors R1881, R1882, R1883, R1884, R1885, and R1886 so that TRACE_CLK and TRACE_D3..0 be routed to the probe.
I downloaded Segger's sample project to check the instruction trace is working, and it does.
But when I try with my own project, I don't have any trace in Ozone (Segger's debugger). The Instruction Trace view displays "No data".
I wrote a JLink script to configure the trace pins on the RT1176 and the clock is output on the TRACE_CLK pin (checked with a scope). So, I suppose the pins are correctly configured.
Do I need to configure something in the ETM? in TPIU? or anywhere else in th RT1176?
Any help will be appreciated.
My experience with this may also be helpful:
https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/MIMXRT1170-EVK-trace-hw-no-present/m-p/1725524#M...
Hi @davidjaouen ,
Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.
I find that you have installed resistors R1881, R1882, R1883, R1884, R1885, and R1886 so that TRACE_CLK and TRACE_D3..0 be routed to the probe.
But I think you still need disconnect other signal resistors on the signal line, such as,
R1290, R1293, R1295, R1294, R1296, which are multiplexed with Ethernet.
I also find a application note for you to refer to.
https://www.nxp.com/webapp/Download?colCode=AN14046&location=null
Wish it helps you.
If you still have question about it, please kindly let me know.
Best Regards
MayLiu