IMXRT1024 UART Terminal Output Issue in Manual Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1024 UART Terminal Output Issue in Manual Configuration

Jump to solution
2,212 Views
Lukas_Frank
Senior Contributor I

Hi all,

 

UART Write and Read operations prints data to terminal screen (serial port configuration) successfully in SDK Pooling Example. But, there is not printing data to terminal screen when I create a project from scratch despite data communication is successfully occur. Why could be my example is not printing to terminal?

 

Thanks and Regards.

0 Kudos
Reply
1 Solution
2,207 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
According to your statement, it seems like the print function doesn't link to UART Write successful, so I was wondering if you can describe the steps you created for a new project in detail.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,208 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
According to your statement, it seems like the print function doesn't link to UART Write successful, so I was wondering if you can describe the steps you created for a new project in detail.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,199 Views
Lukas_Frank
Senior Contributor I

Hi Dear @jeremyzhou,

 

I will try to link them. Then, I'll turn here again.

 

Thanks and Regards.

0 Kudos
Reply