IMXRT1024 UART Terminal Output Issue in Manual Configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMXRT1024 UART Terminal Output Issue in Manual Configuration

跳至解决方案
1,637 次查看
Lukas_Frank
Senior Contributor I

Hi all,

 

UART Write and Read operations prints data to terminal screen (serial port configuration) successfully in SDK Pooling Example. But, there is not printing data to terminal screen when I create a project from scratch despite data communication is successfully occur. Why could be my example is not printing to terminal?

 

Thanks and Regards.

0 项奖励
回复
1 解答
1,632 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
According to your statement, it seems like the print function doesn't link to UART Write successful, so I was wondering if you can describe the steps you created for a new project in detail.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,633 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
According to your statement, it seems like the print function doesn't link to UART Write successful, so I was wondering if you can describe the steps you created for a new project in detail.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
1,624 次查看
Lukas_Frank
Senior Contributor I

Hi Dear @jeremyzhou,

 

I will try to link them. Then, I'll turn here again.

 

Thanks and Regards.

0 项奖励
回复