IMXRT1024 UART Pin Configurations

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMXRT1024 UART Pin Configurations

跳至解决方案
2,805 次查看
Lukas_Frank
Senior Contributor I

Hi all,

 

I am not able to make sense one parameter in IOMUXC_SetPinConfig method in the BOARD_InitPins. It is configValue parameter of IOMUXC_SetPinConfig (sixth-one). I see it assigned as 0x10B0U in the SDK Pooling example. Why? What is the meaning of 0x10B0U. Is there a sheet that explain different combination of this parameter for spesific cases or Is that value constant for all cases?

 

Thanks and Regards.

0 项奖励
回复
1 解答
2,799 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is there a sheet that explains the different combinations of this parameter for specific cases or Is that value constant for all cases?
-- To provide the fastest possible support, I'd highly recommend you to learn the meaning of the 0x10B0U by going through SW_PAD_CTL Register in the RM.
Hope it helps.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,800 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is there a sheet that explains the different combinations of this parameter for specific cases or Is that value constant for all cases?
-- To provide the fastest possible support, I'd highly recommend you to learn the meaning of the 0x10B0U by going through SW_PAD_CTL Register in the RM.
Hope it helps.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
2,792 次查看
Lukas_Frank
Senior Contributor I

Hi Dear @jeremyzhou,

 

There are exactly 2870(SW_PAD_CTL) and 78(0x10B0). I will look the details and turn here again.

 

Thanks and Regards.

0 项奖励
回复