Compatibility of different Arduino shields

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Compatibility of different Arduino shields

跳至解决方案
2,010 次查看
nilz
Contributor II

Hi,

Is the SparkFun Qwiic Shield for Arduino (https://www.sparkfun.com/products/14352) and Grid-EYE® Infrared (IR) Array Sensor Evaluation Kit (https://industry.panasonic.eu/components/sensors/grid-eye/grid-eye-evaluation-kit ) are compatible with NXP i.MX RT1010 Evaluation Kit (https://www.nxp.com/design/development- ... RT1010-EVK)?

Thanks in advance.

标签 (1)
0 项奖励
回复
1 解答
1,996 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

I'd recommend to check the pin layout of both of those devices to make sure  they can be connected directly to the board using the headers. In addition, from checking the protocols used I don't see that you should have any problem using them with the RT1010. However, please consider that the implementation may have to be custom made in the application. As we do not have examples for these directly. 

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,997 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

I'd recommend to check the pin layout of both of those devices to make sure  they can be connected directly to the board using the headers. In addition, from checking the protocols used I don't see that you should have any problem using them with the RT1010. However, please consider that the implementation may have to be custom made in the application. As we do not have examples for these directly. 

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 项奖励
回复