Compatibility of different Arduino shields

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compatibility of different Arduino shields

ソリューションへジャンプ
2,526件の閲覧回数
nilz
Contributor II

Hi,

Is the SparkFun Qwiic Shield for Arduino (https://www.sparkfun.com/products/14352) and Grid-EYE® Infrared (IR) Array Sensor Evaluation Kit (https://industry.panasonic.eu/components/sensors/grid-eye/grid-eye-evaluation-kit ) are compatible with NXP i.MX RT1010 Evaluation Kit (https://www.nxp.com/design/development- ... RT1010-EVK)?

Thanks in advance.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,512件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

I'd recommend to check the pin layout of both of those devices to make sure  they can be connected directly to the board using the headers. In addition, from checking the protocols used I don't see that you should have any problem using them with the RT1010. However, please consider that the implementation may have to be custom made in the application. As we do not have examples for these directly. 

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,513件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

I'd recommend to check the pin layout of both of those devices to make sure  they can be connected directly to the board using the headers. In addition, from checking the protocols used I don't see that you should have any problem using them with the RT1010. However, please consider that the implementation may have to be custom made in the application. As we do not have examples for these directly. 

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 件の賞賛
返信