Bursting supported on SEMC SRAM mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bursting supported on SEMC SRAM mode?

ソリューションへジャンプ
1,015件の閲覧回数
mgarrison
Contributor II

I have set up an RT1064 with SEMC bus connected to an FPGA using the SRAM mode. It is configured for 8-bit, ADMUX, ASYNC mode. When I turn on bursting (at any length) and perform a read, there is no difference in the bus signals. Four independent 8-bit transactions take place, including address phase.  Is this meant to work? It would be a nice way to increase performance since most of our data transfers are 512 bytes.

I did try SYNC mode and can see the difference there on the bus. Is it possible it's not supported in ASYNC mode?

Thanks.

0 件の賞賛
返信
1 解決策
1,007件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @mgarrison ,

ASYNC mode doesn't support burst.

 

Regards,

Jing

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,008件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @mgarrison ,

ASYNC mode doesn't support burst.

 

Regards,

Jing

0 件の賞賛
返信
998件の閲覧回数
mgarrison
Contributor II

Thanks for the quick reply. Please update your documentation. There is no mention of that anywhere.

0 件の賞賛
返信