Boot Code Listing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Boot Code Listing

10,121 次查看
jautry
Contributor IV

I am using an i.MXRT1060 in a custom design but am having boot issues.  It should be copying boot code from QSPI memory to OCRAM and executing, but it is failing and dropping to serial.  I am not using xpresso stuff but eclipse and would like to know if the source of the internal boot code is available for debugging.  I expect the data is getting corrupted in the transfer to memory since the code verifies when loaded into the QSPI flash.

0 项奖励
回复
7 回复数

10,112 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I think I need more information about your design, so I was wondering if you can introduce your testing environment, for instance, a schematic of the board, furthermore, please list the steps of testing in detail.
upload it again.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

10,093 次查看
jautry
Contributor IV

I am using a Segger J-LINK PLUS IF to JTAG in SWD mode to load and verify boot code.  This works fine.  I then check serial port 1 for output on reset and only see a Space to Mark change on the transmit line.  No data transmission is seen.  I think it may be the flash init line of code that is initially loaded that may be wrong but would like to compare the flash content with OCRAM content to see what is transferred.  I just need to find where in OCRAM it puts it.  I assume this is defined in some ivt file.

标记 (1)
0 项奖励
回复

10,087 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your reply and clarification.
According to your proposal, you want to RT1060 boot from the QSPI flash in NON-XIP mode which consists of the below steps (as the below figure shows).
1) Bootable image is in the external flash.
2) loads the starting 4 KB of data from the bootable image to the internal SRAM (OCRAM). It includes the IVT and BD information and will be used for the application image loading.
3) BootROM transfers the starting 4 KB of data from the internal SRAM (OCRAM) to the destination address space of the bootable image.
4) BootROM continues loading the rest of the bootable image from the external flash to the destination address space and starts up the application binary.

jeremyzhou_0-1643253252763.png

To generate a bootable image to implement the above mode, please refer to the post to do it.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

10,053 次查看
jautry
Contributor IV

The problem I am trying to solve is why the boot rom is not executing flash code.  It is hung in a loop:

0x20001A60    0x20001A5A    0x20001AFC

0x20001A7A    0x20001A5C    0x20001AFE

0x20001A7C    0x20001EF4    0x20001B1E

0x20001A7E    0x20001EF6    0x20001EFA

0x20001A74    0x20001AF8    0x20001A60

0x20001A76    0x20001AFA    ...

If anyone has a listing for internal ROM code, what is it looking for??

0 项奖励
回复

10,050 次查看
jautry
Contributor IV

These previous addresses are in the DTCM.  The ROM loop I am seeing is:

0x0020D102 -> 0x0020ED38 ->0020E34C->0x0020E3BA->0x0020E406->0x0020ED48->0x0020D108->

0x0x002173E0->0x0021AA3C->0x002173AE->0x0020D102.

These are all branch points, and am in need of knowing what it is hung on as I cannot find a listing of the internal boot code.

标记 (1)
0 项奖励
回复

10,037 次查看
imxrtuser
Senior Contributor I

Hello jautry,

your problem may come from the gpio boot overrides. Are they set correctly for your flash or do you burn the necessary eFuses?

At least this was my problem when the cpu (IMXRT1020) was hanging in the boot rom memory area. You can check your boot mode and configuration when it hangs in that memory area with the register view of SRC_SBMR2.

Also see chapter GPIO boot overrides and the table with the Fusemap Descriptions if you are not sure what I'm talking about.

Kind regards,

Stefan

0 项奖励
回复

10,030 次查看
jautry
Contributor IV

Thanks for the reply.  Yes, I thought about that.  The values I have are

SBMR1 - 0x00000000

SBMR2 - 0x02000009

 

These appear correct for NOR flash

标记 (1)
0 项奖励
回复