Are external regulators necessary when using i.MX RT1172 Automotive at 800MHz?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Are external regulators necessary when using i.MX RT1172 Automotive at 800MHz?

跳至解决方案
2,532 次查看
Ryo_Aoki
Contributor III

Hi NXP.

The i.MX RT1170 Automotive datasheet states that when (600 MHz < fCM7 ≤ 800 MHz, fCM4 ≤ 400 MHz), the internal DCDC converter is bypassed and an external regulator is required.

Ryo_Aoki_0-1709285634205.png


I believe that an external regulator is required even for i.MX RT1172 (only CM7) at 800MHz, is this understanding correct?
Does the presence or absence of CM4 affect whether an external regulator is required?

 

Best regards.

标记 (1)
0 项奖励
回复
1 解答
2,464 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Your understanding is correct!

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,508 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

The recommendation to use the PMIC or external regulator depends not only on the frequency, but also on the temperature.

You could also find useful the app note AN13213 Using i.MX RT117x Processor with PF5020 PMIC for Auto Application.

Hope it helps you.

Have a nice day!

0 项奖励
回复
2,476 次查看
Ryo_Aoki
Contributor III

Hi Leo.

 

Thank you for your reply.
 -If Tj is below 105 degrees and 800MHz, it can use internal DCDC converter.
 -If Tj is below 125 degrees and 800MHz, it need to use PF5020.
 -And this condition is not affected by the presence or absence of CM4.

This is my understanding, but is this correct?

 

Best regards.

0 项奖励
回复
2,465 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Your understanding is correct!

0 项奖励
回复
2,456 次查看
Ryo_Aoki
Contributor III

It was very helpful.
thank you!

0 项奖励
回复