ADC RT1010

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC RT1010

1,619 Views
gerardo_arriaga
Contributor II

Could someone share a small example of code for the ADC for RT 1010?

Thanks

Labels (1)
2 Replies

1,528 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Gerardo, 

As Daniel stated, within the SDK you will find some ADC examples. You can download the SDK from the following link: Welcome | MCUXpresso SDK Builder 

Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,528 Views
danielmilutinov
Contributor III

Hello Gerardo, 

I haven't tried ADC yet as I'm currently interfacing to a display and keypad. I saw some ADC examples in the SDK, did you have a look at them?