ADC RT1010

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC RT1010

996件の閲覧回数
gerardo_arriaga
Contributor II

Could someone share a small example of code for the ADC for RT 1010?

Thanks

ラベル(1)
2 返答(返信)

905件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Gerardo, 

As Daniel stated, within the SDK you will find some ADC examples. You can download the SDK from the following link: Welcome | MCUXpresso SDK Builder 

Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

905件の閲覧回数
danielmilutinov
Contributor III

Hello Gerardo, 

I haven't tried ADC yet as I'm currently interfacing to a display and keypad. I saw some ADC examples in the SDK, did you have a look at them?