hi
i have created a yocto project,and bitbake core-image-sato, it failed。
the log :
ERROR: core-image-sato-1.0-r0 do_rootfs:
ERROR: ld.so: object '/lib/$LIB/liblsp.so' from /etc/ld.so.preload cannot be preloaded (wrong ELF class: ELFCLASS64): ignored.
NOTE: > Executing update_pixbuf_cache intercept ...
ERROR: ld.so: object '/lib/$LIB/liblsp.so' from /etc/ld.so.preload cannot be preloaded (wrong ELF class: ELFCLASS64): ignored.
NOTE: > Executing update_font_cache intercept ...
ERROR: ld.so: object '/lib/$LIB/liblsp.so' from /etc/ld.so.preload cannot be preloaded (wrong ELF class: ELFCLASS64): ignored.
FC_DEBUG=1
[/home/lyi/imx/fsl-community-bsp/build/tmp/work/imx6ulevk-poky-linux-gnueabi/core-image-sato/1.0-r0/rootfs]/usr/share/fonts: skipping, existing cache is valid: 0 fonts, 1 dirs
[/home/lyi/imx/fsl-community-bsp/build/tmp/work/imx6ulevk-poky-linux-gnueabi/core-image-sato/1.0-r0/rootfs]/usr/share/fonts/ttf: skipping, existing cache is valid: 12 fonts, 0 dirs
Re-scanning [/home/lyi/imx/fsl-community-bsp/build/tmp/work/imx6ulevk-poky-linux-gnueabi/core-image-sato/1.0-r0/rootfs]/usr/share/fonts: caching, new cache contents: 0 fonts, 1 dirs
ERROR: core-image-sato-1.0-r0 do_rootfs: Function failed: do_rootfs
ERROR: Logfile of failure stored in: /home/lyi/imx/fsl-community-bsp/build/tmp/work/imx6ulevk-poky-linux-gnueabi/core-image-sato/1.0-r0/temp/log.do_rootfs.6559
ERROR: Task 9 (/home/lyi/imx/fsl-community-bsp/sources/poky/meta/recipes-sato/images/core-image-sato.bb, do_rootfs) failed with exit code '1'
what's the mean of this error,and hwo to solve ?
thanks for you help!!