where is the secure memory located in i.MX8M Plus?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

where is the secure memory located in i.MX8M Plus?

跳至解决方案
1,209 次查看
tanoue
Contributor III

Hi, everyone.

Please let me know where the secure memory (RAM) is located in i.MX8M Plus.  

The two documents tell me locations of secure memory.

 

i.MX 8M Plus Applications Processor Datasheet for Consumer Products (IMX8MPCEC)

According to CAAM in Modules list, the following sentence is written.

"In i.MX 8M Plus processors, the secure memory provided is 32 KB."

 

Security Reference Manual for i.MX 8M Plus Applications Processor (IMX8MPSRM)

I can't write the details because it is an NDA document, but it says the following.

・SNVS includes On-chip secure RAM (32 KB)

・A figure shows that CAAM includes Secure RAM

 

Is the both modules have secure memory?

Or only one or the other?

 

Best Regards.

0 项奖励
回复
1 解答
1,203 次查看
Yuri
NXP Employee
NXP Employee

@tanoue 
Hello,

   I've sent some comment directly.

Regards,
Yuri.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,204 次查看
Yuri
NXP Employee
NXP Employee

@tanoue 
Hello,

   I've sent some comment directly.

Regards,
Yuri.

0 项奖励
回复