where is the secure memory located in i.MX8M Plus?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

where is the secure memory located in i.MX8M Plus?

ソリューションへジャンプ
1,234件の閲覧回数
tanoue
Contributor III

Hi, everyone.

Please let me know where the secure memory (RAM) is located in i.MX8M Plus.  

The two documents tell me locations of secure memory.

 

i.MX 8M Plus Applications Processor Datasheet for Consumer Products (IMX8MPCEC)

According to CAAM in Modules list, the following sentence is written.

"In i.MX 8M Plus processors, the secure memory provided is 32 KB."

 

Security Reference Manual for i.MX 8M Plus Applications Processor (IMX8MPSRM)

I can't write the details because it is an NDA document, but it says the following.

・SNVS includes On-chip secure RAM (32 KB)

・A figure shows that CAAM includes Secure RAM

 

Is the both modules have secure memory?

Or only one or the other?

 

Best Regards.

0 件の賞賛
返信
1 解決策
1,228件の閲覧回数
Yuri
NXP Employee
NXP Employee

@tanoue 
Hello,

   I've sent some comment directly.

Regards,
Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,229件の閲覧回数
Yuri
NXP Employee
NXP Employee

@tanoue 
Hello,

   I've sent some comment directly.

Regards,
Yuri.

0 件の賞賛
返信