where is the secure memory located in i.MX8M Plus?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

where is the secure memory located in i.MX8M Plus?

Jump to solution
1,238 Views
tanoue
Contributor III

Hi, everyone.

Please let me know where the secure memory (RAM) is located in i.MX8M Plus.  

The two documents tell me locations of secure memory.

 

i.MX 8M Plus Applications Processor Datasheet for Consumer Products (IMX8MPCEC)

According to CAAM in Modules list, the following sentence is written.

"In i.MX 8M Plus processors, the secure memory provided is 32 KB."

 

Security Reference Manual for i.MX 8M Plus Applications Processor (IMX8MPSRM)

I can't write the details because it is an NDA document, but it says the following.

・SNVS includes On-chip secure RAM (32 KB)

・A figure shows that CAAM includes Secure RAM

 

Is the both modules have secure memory?

Or only one or the other?

 

Best Regards.

0 Kudos
Reply
1 Solution
1,232 Views
Yuri
NXP Employee
NXP Employee

@tanoue 
Hello,

   I've sent some comment directly.

Regards,
Yuri.

View solution in original post

0 Kudos
Reply
1 Reply
1,233 Views
Yuri
NXP Employee
NXP Employee

@tanoue 
Hello,

   I've sent some comment directly.

Regards,
Yuri.

0 Kudos
Reply