vddpu VPU/GPU Power

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,968件の閲覧回数
lifusong
Contributor IV

Dear sir.

  our board is base imx6Q , android BSP is 4.4.3_r1  Kernel version is 3.10.53 uboot version is 2014.04

why the

reg_pu: regulator-vddpu@140 {

only have voltage is 0.2v.

bud the android 4.2.2 code ,this pin's voltage is 1.265V.

any body can help me?

thans very much!

0 件の賞賛
返信
1 解決策
1,763件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi li

reason may be that at start-up vddpu regulator is gated,

however if you run application which uses gpu, it should be turned

on, please check that.  Android 4.4.3 uses different kernel version than

android 4.2.2, so behaviour is different.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,764件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi li

reason may be that at start-up vddpu regulator is gated,

however if you run application which uses gpu, it should be turned

on, please check that.  Android 4.4.3 uses different kernel version than

android 4.2.2, so behaviour is different.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信