vddpu VPU/GPU Power

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

vddpu VPU/GPU Power

Jump to solution
1,918 Views
lifusong
Contributor IV

Dear sir.

  our board is base imx6Q , android BSP is 4.4.3_r1  Kernel version is 3.10.53 uboot version is 2014.04

why the

reg_pu: regulator-vddpu@140 {

only have voltage is 0.2v.

bud the android 4.2.2 code ,this pin's voltage is 1.265V.

any body can help me?

thans very much!

0 Kudos
Reply
1 Solution
1,713 Views
igorpadykov
NXP Employee
NXP Employee

Hi li

reason may be that at start-up vddpu regulator is gated,

however if you run application which uses gpu, it should be turned

on, please check that.  Android 4.4.3 uses different kernel version than

android 4.2.2, so behaviour is different.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,714 Views
igorpadykov
NXP Employee
NXP Employee

Hi li

reason may be that at start-up vddpu regulator is gated,

however if you run application which uses gpu, it should be turned

on, please check that.  Android 4.4.3 uses different kernel version than

android 4.2.2, so behaviour is different.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply