vddpu VPU/GPU Power

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

vddpu VPU/GPU Power

跳至解决方案
1,893 次查看
lifusong
Contributor IV

Dear sir.

  our board is base imx6Q , android BSP is 4.4.3_r1  Kernel version is 3.10.53 uboot version is 2014.04

why the

reg_pu: regulator-vddpu@140 {

only have voltage is 0.2v.

bud the android 4.2.2 code ,this pin's voltage is 1.265V.

any body can help me?

thans very much!

0 项奖励
回复
1 解答
1,688 次查看
igorpadykov
NXP Employee
NXP Employee

Hi li

reason may be that at start-up vddpu regulator is gated,

however if you run application which uses gpu, it should be turned

on, please check that.  Android 4.4.3 uses different kernel version than

android 4.2.2, so behaviour is different.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,689 次查看
igorpadykov
NXP Employee
NXP Employee

Hi li

reason may be that at start-up vddpu regulator is gated,

however if you run application which uses gpu, it should be turned

on, please check that.  Android 4.4.3 uses different kernel version than

android 4.2.2, so behaviour is different.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复