v4l2src USB Raw camera stream pipeline

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

v4l2src USB Raw camera stream pipeline

1,767 次查看
hpdwally
Contributor II

I purchased an Aptina MT9M021 from leopard (LI-USB30-M021) that streams RAW.

I was able to setup viewing of the stream with mplayer, and gst-launch-0.10 as well but the video output was green. I understand that the color space conversion is not happening correctly, and was wondering if anyone else has figured out in the pipeline commands how to get the image to covert properly.

I do have the option to get a YUV coverted output as well, and probably will, but it would be nice to be able to use this sensor if possible.

0 项奖励
回复
2 回复数

1,266 次查看
BrilliantovKiri
Senior Contributor I

Hello, Johnny!

I use follow pipeline with OmniVision OV2715:

gst-launch mfw_v4lsrc capture-format=2 capture-width=1280 capture-height=720 ! bayer2rgb ! ffmpegcolorspace ! mfw_vpuencoder codec-type=std_avc ! rtph264pay pt=96 ! udpsink host=224.1.4.6 port=5000 sync=false -v

0 项奖励
回复

1,266 次查看
LeonardoSandova
Specialist I

have you tried v4l2src ! mfw_ipucsc ! mfw_v4lsink ?

Leo

0 项奖励
回复