v4l2src USB Raw camera stream pipeline

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

v4l2src USB Raw camera stream pipeline

2,277件の閲覧回数
hpdwally
Contributor II

I purchased an Aptina MT9M021 from leopard (LI-USB30-M021) that streams RAW.

I was able to setup viewing of the stream with mplayer, and gst-launch-0.10 as well but the video output was green. I understand that the color space conversion is not happening correctly, and was wondering if anyone else has figured out in the pipeline commands how to get the image to covert properly.

I do have the option to get a YUV coverted output as well, and probably will, but it would be nice to be able to use this sensor if possible.

0 件の賞賛
返信
2 返答(返信)

1,776件の閲覧回数
BrilliantovKiri
Senior Contributor I

Hello, Johnny!

I use follow pipeline with OmniVision OV2715:

gst-launch mfw_v4lsrc capture-format=2 capture-width=1280 capture-height=720 ! bayer2rgb ! ffmpegcolorspace ! mfw_vpuencoder codec-type=std_avc ! rtph264pay pt=96 ! udpsink host=224.1.4.6 port=5000 sync=false -v

0 件の賞賛
返信

1,776件の閲覧回数
LeonardoSandova
Specialist I

have you tried v4l2src ! mfw_ipucsc ! mfw_v4lsink ?

Leo

0 件の賞賛
返信