Hi Sagar,
As Mrudang Shelat above rely, Both the two routing topologies can work for 2 x DDR3L with the iMX6Q processor. But here recommend you to use the T-Topology, as the same as our reference design.
Have a nice day
Rita
Hi Sagar,
If you are using the PMIC, you also need to confirm that if your DDR3L compatible to 1.5V. If yes, you can directly use the MMPF0100F0EP. If it not compatible to 1.5V, you need to use the MMPF0100NPAEP, and modify the F0 code by changing the SW3 output to 1.35V from 1.5V.
Have a great day,
Rita
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Sagar,
As Mrudang Shelat above rely, Both the two routing topologies can work for 2 x DDR3L with the iMX6Q processor. But here recommend you to use the T-Topology, as the same as our reference design.
Have a nice day
Rita
Hi Sagar,
You can use both the routing topologies for 2 x DDR3L with the iMX6Q processor.
Also, see reference: https://community.nxp.com/message/826962
Regards