Hi
I am using i.MX6 Quad Processor and two DDR3L of 512Mx16 configuration. Please let me know if processor supports fly-by topology. Or do we have to use T-Topology only. Kindly clarify
Thanks
Sagar
Solved! Go to Solution.
Hi Sagar,
As Mrudang Shelat above rely, Both the two routing topologies can work for 2 x DDR3L with the iMX6Q processor. But here recommend you to use the T-Topology, as the same as our reference design.
Have a nice day
Rita
Hi Sagar,
If you are using the PMIC, you also need to confirm that if your DDR3L compatible to 1.5V. If yes, you can directly use the MMPF0100F0EP. If it not compatible to 1.5V, you need to use the MMPF0100NPAEP, and modify the F0 code by changing the SW3 output to 1.35V from 1.5V.
Have a great day,
Rita
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Rita
Thanks for your valuable suggestion. I am using MMPF0100F6AEP for DDR3L power supply. Its SW3 O/P is capable of providing 1.35V.
Thanks
Sagar
Hi Sagar,
I am very glad it can do help for you.If you have new questions , you can create new thread and contact us.
Have a nice day
Best Regards
Rita
Hi Sagar,
As Mrudang Shelat above rely, Both the two routing topologies can work for 2 x DDR3L with the iMX6Q processor. But here recommend you to use the T-Topology, as the same as our reference design.
Have a nice day
Rita
Hi Sagar,
You can use both the routing topologies for 2 x DDR3L with the iMX6Q processor.
Also, see reference: https://community.nxp.com/message/826962
Regards