usb host2 of the imx27 with isp1504.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usb host2 of the imx27 with isp1504.

885 Views
731378628
Contributor I

Hello, I have encountered a problem when debugging the usx host2 of the imx27. In the hardware circuit, the processor communicates with the usb interface through the chip isp1504. In my test, after configuring each pin, but not successfully setting up the isp1504 program, the phrase “while (__raw_readl(view) & ULPIVW_RUN) never exits, and I see that the manual is cleared automatically. I think it may be a driving problem. Can I give me a corresponding drive?

0 Kudos
Reply
1 Reply

833 Views
igorpadykov
NXP Employee
NXP Employee

Hi gao

please create service request for obtaining additional materials.

How to create service request :
https://community.nxp.com/docs/DOC-329745 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply