uboot defconfig for iMX8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uboot defconfig for iMX8

Jump to solution
5,761 Views
davidvescovi
Contributor V

maybe I am just too old school but I can not for the life of me find the u-boot xxx_defconfig for the iMX8.

I am use to seeing a file like imx6q_logic_defconfig in the uboot-imx/configs folder for the evk boards.

Even the latest "i.MX porting guide" explains it this way.

I need to create a custom uboot for our board that is based off of the iMX8m mini evk.

I cloned the imx_v2018.03_4.14.98_2.0.0_ga uboot-imx.

Maybe I am looking in the wrong place, where should I be looking?

Tags (1)
0 Kudos
Reply
1 Solution
5,286 Views
davidvescovi
Contributor V

silly me I checked out imx_4.14.98_2.1.0 its not there.

its in rel_imx_4.14.98_2.1.0

View solution in original post

0 Kudos
Reply
3 Replies
5,230 Views
fei_4_xu
Contributor III

I would suggest to read this document instead:

i.MX8 Boot process and creating a bootable image

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-Boot-process-and-creating-a-bootab...

 

0 Kudos
Reply
5,287 Views
davidvescovi
Contributor V

silly me I checked out imx_4.14.98_2.1.0 its not there.

its in rel_imx_4.14.98_2.1.0

0 Kudos
Reply
5,286 Views
igorpadykov
NXP Employee
NXP Employee

Hi David

one can look at toradex tutorial:

Build Apalis iMX8/Colibri iMX8X Boot Image/Linux from Scratch 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply