uboot defconfig for iMX8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

uboot defconfig for iMX8

跳至解决方案
5,767 次查看
davidvescovi
Contributor V

maybe I am just too old school but I can not for the life of me find the u-boot xxx_defconfig for the iMX8.

I am use to seeing a file like imx6q_logic_defconfig in the uboot-imx/configs folder for the evk boards.

Even the latest "i.MX porting guide" explains it this way.

I need to create a custom uboot for our board that is based off of the iMX8m mini evk.

I cloned the imx_v2018.03_4.14.98_2.0.0_ga uboot-imx.

Maybe I am looking in the wrong place, where should I be looking?

标记 (1)
0 项奖励
回复
1 解答
5,292 次查看
davidvescovi
Contributor V

silly me I checked out imx_4.14.98_2.1.0 its not there.

its in rel_imx_4.14.98_2.1.0

在原帖中查看解决方案

0 项奖励
回复
3 回复数
5,236 次查看
fei_4_xu
Contributor III

I would suggest to read this document instead:

i.MX8 Boot process and creating a bootable image

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-Boot-process-and-creating-a-bootab...

 

0 项奖励
回复
5,293 次查看
davidvescovi
Contributor V

silly me I checked out imx_4.14.98_2.1.0 its not there.

its in rel_imx_4.14.98_2.1.0

0 项奖励
回复
5,292 次查看
igorpadykov
NXP Employee
NXP Employee

Hi David

one can look at toradex tutorial:

Build Apalis iMX8/Colibri iMX8X Boot Image/Linux from Scratch 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复