u-boot.imx dcd table size

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

u-boot.imx dcd table size

跳至解决方案
3,327 次查看
xiongweihuang
Contributor III

Hello all

I get the source from http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/log/?h=imx_v2013.04_3.10.17_1.0.0_beta

And after build with several boards config

I notice you get the u-boot.bin from 32k offset in u-boot.imx

Is there any special reason for this ?

With previous version , you start the real u-boot code from 1k offset

How Freescale boot rom support boot from different offset ?

or

Is this a bug ?

标记 (4)
0 项奖励
回复
1 解答
2,658 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
6 回复数
2,659 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
2,658 次查看
xiongweihuang
Contributor III

Thanks Yixing

Please close this

Regards

0 项奖励
回复
2,658 次查看
YixingKong
Senior Contributor IV

Weihuang

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 项奖励
回复
2,658 次查看
JasonZhao
Contributor V

Hi, xiongweihuang

Where do you find the 32k offset, As I know, there is 20KB offset in 2013.04, the true u-boot code locate in 0x5000.

0 项奖励
回复
2,658 次查看
YixingKong
Senior Contributor IV

JasonZhao, could you help this customer's question please?

Thanks,

Yixing

0 项奖励
回复
2,658 次查看
Wlodek_D_
Senior Contributor II

Dear xiongweihuang,

Thank you for your post, however please consider moving it to the right community place for better visibility.

For details please see general advice https://community.freescale.com/docs/DOC-99909

Thank you for using Freescale Community.

Regards,

Wlodek_D.

0 项奖励
回复