u-boot.imx dcd table size

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

u-boot.imx dcd table size

ソリューションへジャンプ
4,790件の閲覧回数
xiongweihuang
Contributor III

Hello all

I get the source from http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/log/?h=imx_v2013.04_3.10.17_1.0.0_beta

And after build with several boards config

I notice you get the u-boot.bin from 32k offset in u-boot.imx

Is there any special reason for this ?

With previous version , you start the real u-boot code from 1k offset

How Freescale boot rom support boot from different offset ?

or

Is this a bug ?

タグ(4)
0 件の賞賛
返信
1 解決策
4,121件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
4,122件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
4,121件の閲覧回数
xiongweihuang
Contributor III

Thanks Yixing

Please close this

Regards

0 件の賞賛
返信
4,121件の閲覧回数
YixingKong
Senior Contributor IV

Weihuang

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛
返信
4,121件の閲覧回数
JasonZhao
Contributor V

Hi, xiongweihuang

Where do you find the 32k offset, As I know, there is 20KB offset in 2013.04, the true u-boot code locate in 0x5000.

0 件の賞賛
返信
4,121件の閲覧回数
YixingKong
Senior Contributor IV

JasonZhao, could you help this customer's question please?

Thanks,

Yixing

0 件の賞賛
返信
4,121件の閲覧回数
Wlodek_D_
Senior Contributor II

Dear xiongweihuang,

Thank you for your post, however please consider moving it to the right community place for better visibility.

For details please see general advice https://community.freescale.com/docs/DOC-99909

Thank you for using Freescale Community.

Regards,

Wlodek_D.

0 件の賞賛
返信