trouble booting linux kernel for imx6ull

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

trouble booting linux kernel for imx6ull

4,259件の閲覧回数
haithemsmida
Contributor I

Hello every body,

I just started integration of an im6uLL board, trying some test with an evk board.

I'd like to compile a linux kernel and use it, but the kernel doesn't boot and freeze

here is the detail of what i tried:

downloading kernel source from: linux-imx.git - i.MX Linux Kernel (4.1.15_2.0.0 GA)

create a sid chroot

use the sid chroot and add architecture armhf

installing arm-toolchain  arm-linux-gnueabihf

export ARCH=arm

export CROSS_COMPILE=arm-linux-gnueabihf-

make menuconfig , and activate imx6ull support 

make 

copy the new zImage and imx6ull-14x14-evk.dtb  on the microSD

fatload mmc 1:1 0x83000000  imx6ull-14x14-evk.dtb

fatload mmc 1:1 0x80800000 zImage

bootz 0x80800000 - 0x83000000

After calling  bootz, and entring  kernel_entry(0, machid, r2); in boot_jump_linux , 

the linux kernel freeze  with no debug trace.

i tried also the use the predefined config  : imx_v6_v7_defconfig

make imx_v6_v7_defconfig

make 

but I get compilation error :undefined reference to `mxc_dispdrv_gethandle'

seems strange the support of this board !

could any one please help me figure out what's going on.

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

3,522件の閲覧回数
jian_jiang
NXP Employee
NXP Employee

Hi haithem,

You may use the imx_v7_defconfig to have a try.

Or you can build a Yocto Project and use the MFG Tools to download the uboot, kernel, dtb and rootfs according to the doc attached by igor.

All the Best

Kane

0 件の賞賛
返信

3,515件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi haithem

please follow attached Yocto Guide sect.5 Image Build

and Linux Guide for bootitng. More documentation can be found on

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信