trouble booting linux kernel for imx6ull

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

trouble booting linux kernel for imx6ull

5,485 次查看
haithemsmida
Contributor I

Hello every body,

I just started integration of an im6uLL board, trying some test with an evk board.

I'd like to compile a linux kernel and use it, but the kernel doesn't boot and freeze

here is the detail of what i tried:

downloading kernel source from: linux-imx.git - i.MX Linux Kernel (4.1.15_2.0.0 GA)

create a sid chroot

use the sid chroot and add architecture armhf

installing arm-toolchain  arm-linux-gnueabihf

export ARCH=arm

export CROSS_COMPILE=arm-linux-gnueabihf-

make menuconfig , and activate imx6ull support 

make 

copy the new zImage and imx6ull-14x14-evk.dtb  on the microSD

fatload mmc 1:1 0x83000000  imx6ull-14x14-evk.dtb

fatload mmc 1:1 0x80800000 zImage

bootz 0x80800000 - 0x83000000

After calling  bootz, and entring  kernel_entry(0, machid, r2); in boot_jump_linux , 

the linux kernel freeze  with no debug trace.

i tried also the use the predefined config  : imx_v6_v7_defconfig

make imx_v6_v7_defconfig

make 

but I get compilation error :undefined reference to `mxc_dispdrv_gethandle'

seems strange the support of this board !

could any one please help me figure out what's going on.

标签 (2)
0 项奖励
回复
2 回复数

4,748 次查看
jian_jiang
NXP Employee
NXP Employee

Hi haithem,

You may use the imx_v7_defconfig to have a try.

Or you can build a Yocto Project and use the MFG Tools to download the uboot, kernel, dtb and rootfs according to the doc attached by igor.

All the Best

Kane

0 项奖励
回复

4,741 次查看
igorpadykov
NXP Employee
NXP Employee

Hi haithem

please follow attached Yocto Guide sect.5 Image Build

and Linux Guide for bootitng. More documentation can be found on

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复