some questions about the use of the HAB in imx6 ROM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

some questions about the use of the HAB in imx6 ROM

跳至解决方案
804 次查看
guokaizhao
Contributor I

(1)Whether The program in ROM which use the HAB run in trustzone.

(2)Is IMX6 on-chip ROM program fixed in factory, or we can customize it ourselves.If we can customize the programs in the ROM, can you provide the sample source code for customize.

(3)If The ROM program which use the HAB operation on-chip resources will conflict with the following initialization in uboot and Linux kernel.

标签 (1)
0 项奖励
回复
1 解答
728 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please look at my comments below.

 

1.
The boot ROM works in secure world.

 

2.

  The boot ROM is mask programmed and cannot be changed by customers.

 

3.

  The HAB boot is used to load U-boot, and boot ROM configuration can be
reprogrammed by U-boot.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
729 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please look at my comments below.

 

1.
The boot ROM works in secure world.

 

2.

  The boot ROM is mask programmed and cannot be changed by customers.

 

3.

  The HAB boot is used to load U-boot, and boot ROM configuration can be
reprogrammed by U-boot.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复