some questions about the use of the HAB in imx6 ROM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

some questions about the use of the HAB in imx6 ROM

Jump to solution
902 Views
guokaizhao
Contributor I

(1)Whether The program in ROM which use the HAB run in trustzone.

(2)Is IMX6 on-chip ROM program fixed in factory, or we can customize it ourselves.If we can customize the programs in the ROM, can you provide the sample source code for customize.

(3)If The ROM program which use the HAB operation on-chip resources will conflict with the following initialization in uboot and Linux kernel.

Labels (1)
0 Kudos
Reply
1 Solution
826 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please look at my comments below.

 

1.
The boot ROM works in secure world.

 

2.

  The boot ROM is mask programmed and cannot be changed by customers.

 

3.

  The HAB boot is used to load U-boot, and boot ROM configuration can be
reprogrammed by U-boot.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
827 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please look at my comments below.

 

1.
The boot ROM works in secure world.

 

2.

  The boot ROM is mask programmed and cannot be changed by customers.

 

3.

  The HAB boot is used to load U-boot, and boot ROM configuration can be
reprogrammed by U-boot.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply