second bootsource

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

second bootsource

跳至解决方案
1,956 次查看
chris321
Contributor IV

Hello Community,

Is it possible to force the i.MX28 to boot with the USB recovery mode before it tries the SSP0?

I think something like

I.mx28 power on --> usb recovery mode --> any mfgtool for update there?  ...

(yes) --> update

(no) --> boot from SD(eMMC)

one possible solution I have found is to set at every boot a HW_RTC_PERSISTENT bit to boot at the next boot in usb recovery mode but is there any other way?

best regards

标签 (1)
0 项奖励
回复
1 解答
1,801 次查看
igorpadykov
NXP Employee
NXP Employee

Hi chris321

I am afraid there are no ways to force processor for such kind of boot flow.

Best regards

igor

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,802 次查看
igorpadykov
NXP Employee
NXP Employee

Hi chris321

I am afraid there are no ways to force processor for such kind of boot flow.

Best regards

igor

0 项奖励
回复