second bootsource

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

second bootsource

Jump to solution
2,046 Views
chris321
Contributor IV

Hello Community,

Is it possible to force the i.MX28 to boot with the USB recovery mode before it tries the SSP0?

I think something like

I.mx28 power on --> usb recovery mode --> any mfgtool for update there?  ...

(yes) --> update

(no) --> boot from SD(eMMC)

one possible solution I have found is to set at every boot a HW_RTC_PERSISTENT bit to boot at the next boot in usb recovery mode but is there any other way?

best regards

Labels (1)
0 Kudos
Reply
1 Solution
1,891 Views
igorpadykov
NXP Employee
NXP Employee

Hi chris321

I am afraid there are no ways to force processor for such kind of boot flow.

Best regards

igor

View solution in original post

0 Kudos
Reply
1 Reply
1,891 Views
igorpadykov
NXP Employee
NXP Employee

Hi chris321

I am afraid there are no ways to force processor for such kind of boot flow.

Best regards

igor

0 Kudos
Reply