second bootsource

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,958件の閲覧回数
chris321
Contributor IV

Hello Community,

Is it possible to force the i.MX28 to boot with the USB recovery mode before it tries the SSP0?

I think something like

I.mx28 power on --> usb recovery mode --> any mfgtool for update there?  ...

(yes) --> update

(no) --> boot from SD(eMMC)

one possible solution I have found is to set at every boot a HW_RTC_PERSISTENT bit to boot at the next boot in usb recovery mode but is there any other way?

best regards

ラベル(1)
0 件の賞賛
返信
1 解決策
1,803件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi chris321

I am afraid there are no ways to force processor for such kind of boot flow.

Best regards

igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,804件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi chris321

I am afraid there are no ways to force processor for such kind of boot flow.

Best regards

igor

0 件の賞賛
返信